Merry Boxes & LEDs

Enter Your Project for a chance to win a Maker Tool Kit, an Oscilloscope Grand Prize for the project that brings the Most Joy to the Heart, and Gift to Gives!

Back to The Project14 homepage

Project14 Home
Monthly Themes
Monthly Theme Poll

 

 

ESP-Now device for warning of the approach of Santa!  This device has a Master which detects with PIR or a wire break to set a pin low--it is monitored when a TPL 5111 wakes the unit up.  The solar charger keeps the device charged with a battery mounted on the roof.  The receiver device (Slave) constantly monitors for the ESP-Now communication from the master and announces the arrival of St. Nick with a bright cascade of Led's.