Skip navigation
1 2 Previous

Programmable Logic

19 posts
The Arduino MKR Vidor 4000 is a powerful but also mysterious board. The FPGA gives it a performance boost over other Arduinos but its functions are very badly documented. There are also very few code examples available on the internet.   Mini PCIe connector of the Vidor  I took a closer look at the Mini PCIe connector and wanted to see which functions are available at these pins.   This connector has 52 positions and the pinout can be grabbed from the official schematics of the ...
rsc

MKR VIDOR 4000 Simple DVM

Posted by rsc Jul 16, 2019
Programmable Logic Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   Here's a simple DVM made from an Arduino VIDOR 4000. A potentiometer is placed in between VCC and GND with the wiper connected to analog input A3. The value of the analog input is read and then shown through the HDMI to a monitor screen. The arduino example code for showing the Ardu ...
Programmable Logic Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll     What is FPGA? (source: Wikipedia) A field-programmable gate array (FPGA) is an integrated circuit designed to be configured by a customer or a designer after manufacturing – hence the term "field-programmable". The FPGA configuration is generally specified using a hardw ...
Programmable Logic Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   SMART CYCLE     SUMMARY   In today’s world everything is being revolutionised and technological advancements are made everyday to day objects smarter so why not our cycles?Cyclists and motorists are the most likely to be killed or injured on the road as fatality ra ...
Programmable Logic Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   When you build robots you always have to control lots of motors or RC servos. If you use a micro controller as main computing device you are fine because these devices have plenty of PWM outputs to control motors. But when you switch to more powerful controllers like the Raspberry Pi o ...
Programmable Logic Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   Introduction       'Programmable Logic' Project14 competition has given Element14 Community members (and myself) a chance to explore 'Programmable Logic' which is usually not explored by hobbyists or makers in the first place. This may be due to the code or hard ...
Programmable Logic Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   VidorScout Assembly and Test  Related Posts VidorScout - MKR Vidor 4000 Mobile Robot: Intro VidorScout - MKR Vidor 4000 Mobile Robot: VidorBitstream compile VidorScout - MKR Vidor 4000 Mobile Robot: Camera QR Code Recognition   The VidorScout is a mobile robot that self nav ...
Programmable Logic Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   My basic idea is to use Arduino MKR4000 board as source of true random generator for calculation based on Monte Carlo methods. At first stage of getting familiar with this board and Quartus software I have created a simple pseudo random generator which uses linear feedback shift regi ...
Programmable Logic Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   This month's Project14 | Build Projects that Use a Programmable Logic Device such as FPGA or CPLD! theme comes after almost a year since I first started working with FPGAs. While the project at its current stage does not make use of the ARM core in the Zynq, I managed to make use of a ...
Programmable Logic Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   Hi folks, during my master's degree on computer science, i worked on the development of an architecture for checking digital circuits, based on FPGA focused on data centers, and high performance systems. But due to lack of support from the developers and the final cost of the FPGA using ...
Programmable Logic Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   So, I've decided what I'm going to do for my Programmable Logic Project 14 entry. It's going to be a ball-rolling sort of game controlled by a couple of micro:bits. I'm hoping my kids will be able to help with the micro:bit side of things.   As the FPGA (a Spartan 7 on an Arty S7 ...
Programmable Logic Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   MKR Vidor 4000 Camera Example   The Arduino MKR Vidor 4000 is not only the first in the Arduino MKR series to provide a FPGA option, it also as the option to add a camera via a MIPI connector near the Mini PCIe connector.  With the assistance of the onboard FPGA, this allows ...
Programmable Logic Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   This month's Projec14 - Programmable Logic - really appeals to me because I'm trying to get in FPGAs, but I'm finding it a little hard going. Well, let's be honest it's not easy. It's the sort of thing that I understand when i read it, I understand when i try it, but I struggle with wh ...
Programmable Logic Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   VidorBitstream  Part of the intent of the VidorScout project is to take advantage of the FPGA code that Arduino has provided and modify it for a particular purpose.  It is unknown at this time whether this is possible since not all of the released FPGA code has been provided ...
Programmable Logic Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   Overview  VidorScout is an autonomous mobile robot that uses Sensor Fusion which combines camera vision, Time of Flight Sensor data and IR Sensors to identify objects for both avoidance and for object identification. The camera sensor can also be used for QR code identification to ...