Skip navigation
The Arduino MKR Vidor 4000 is a powerful but also mysterious board. The FPGA gives it a performance boost over other Arduinos but its functions are very badly documented. There are also very few code examples available on the internet.   Mini PCIe connector of the Vidor  I took a closer look at the Mini PCIe connector and wanted to see which functions are available at these pins.   This connector has 52 positions and the pinout can be grabbed from the official schematics of the ...