Skip navigation

Programmable Logic

4 Posts authored by: jomoenginer
Programmable Logic Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   VidorScout Assembly and Test  Related Posts VidorScout - MKR Vidor 4000 Mobile Robot: Intro VidorScout - MKR Vidor 4000 Mobile Robot: VidorBitstream compile VidorScout - MKR Vidor 4000 Mobile Robot: Camera QR Code Recognition   The VidorScout is a mobile robot that self nav ...
Programmable Logic Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   MKR Vidor 4000 Camera Example   The Arduino MKR Vidor 4000 is not only the first in the Arduino MKR series to provide a FPGA option, it also as the option to add a camera via a MIPI connector near the Mini PCIe connector.  With the assistance of the onboard FPGA, this allows ...
Programmable Logic Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   VidorBitstream  Part of the intent of the VidorScout project is to take advantage of the FPGA code that Arduino has provided and modify it for a particular purpose.  It is unknown at this time whether this is possible since not all of the released FPGA code has been provided ...
Programmable Logic Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   Overview  VidorScout is an autonomous mobile robot that uses Sensor Fusion which combines camera vision, Time of Flight Sensor data and IR Sensors to identify objects for both avoidance and for object identification. The camera sensor can also be used for QR code identification to ...