Remote Monitoring & Control

Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product!

Back to The Project14 homepage

Project14 Home
Monthly Themes
Monthly Theme Poll

 

Assaulting the cloud: uploading fitness data to IoT

 

The hardware is pretty straight forward:

 

a. power:

- 18650 battery

- a TP4056 battery-charger unit;

- a DC-DC boost convert to 5V.

 

b. controller:

- a ESP8266 D1 mini board.

 

c. display and user interaction:

- a regular 1602 LCD (HD44780 controlled);

- a PCF8574ATPCF8574AT I2C adapter.

- UPLOAD button;

- SELECT button - to select between displaying mode: either TIME, CALORIES, DISTANCE, RPM or ALL (this is not yet implemented). Currently ALL are displayed at once;

- UP and DOWN buttons - to increase/decrease number of minutes for workout - it is not yet implemented.

 

I have improvised a shield for D1 mini: all signals from buttons and LCD come to the shield via 10-pin flat ribbon cable. This way I can detach the parts of the console and open it quite easily. Also on the shield I have two connectors: one for the sensor and one for the POWER switch.

 

Routing the wires inside the console enclosure and fitting everything inside proved to be a more challenging than I originally thought. I see how easily (and more elegant) it would have been to 3D print an enclosure especially for this.

 

As far as software is concerned:

 

- the bike can measure the time for workout, distance traveled, RPM, average speed for the whole workout (meters/seconds);

- all the data is uploaded to Thingspeak once the UPLOAD button is pressed;

- since the ESP8266 is located in a place that is not easily accesible, OTA (Over The Air) updating is included in the software.

 

 

What needs to be added:

 

-  calories measurement;

-  use a bigger font to display one of the metrics;

-  different predefined workouts (selectable).

 

Pictures of the console (this is the back side of the console, the side that is not visible to the user): the ribbon coming from inside the console, the sensor wires and the power switch wires.

 

control unit for the bike

 

For charging the battery:

control unit for the bike - charging

 

Data on Thingspeak:

 

control unit for the bike - data on thingspeak