Skip navigation
Month of Robots Enter Your Project for a chance to win robot prizes for your robot builds and a $200 shopping cart!  The Birthday Special: Robot Prizes for Robot Projects! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll     This is a bit late, but I wanted to get an update with my PWHBot based on what I have. Related Posts: PWHBot #1: Introduction   I've added the LM339 IR Sensor Array to the bot and placed the sensors at the end of some ...
mcb1

HaloBOT ver 2.0

Posted by mcb1 Top Member May 13, 2018
Robots with Wheels Enter Your Electronics & Design Project for Your Chance to Win a $100 Shopping Cart! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   Some time ago my daughter and I built a robot based on Picaxe. It got named HaloBOT and the build is here HaloBOT   Picaxe was chosen at the time to allow Hayley to use the Flowchart version of programming, and it was based ona  single board, rather than a collection of bits. It works a ...
Robots with Wheels Enter Your Electronics & Design Project for Your Chance to Win a $100 Shopping Cart! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   Hello everyone, I saw the Project14 theme of this month and i was really intrigued with sharing my work with the community. lately i have been working on robotic systems including robotic arms and unmanned vehicles and i would love to share the project with everyone.   INTRODUCTION:- the post ...
Robots with Wheels Enter Your Electronics & Design Project for Your Chance to Win a $100 Shopping Cart! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   The journey for RoboBobLet for the Robot with Wheels challenge has come to an end for me as there is no more time left. I added V53L0X laser rangefinder to the 3D printed front piece added to the front of the Pixy camera and connected everything to the Nano. Apart from one head-scratching moment when ...
Robots with Wheels Enter Your Electronics & Design Project for Your Chance to Win a $100 Shopping Cart! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   Another step towards the completion of RoboBobLet is to add a camera system. It would be possible to add a simpler digital camera to RoboBobLet and then use the Arduino to do some simple image processing but that would take more time than is available. An alternative is to use the Pixy Camera system ...