Skip navigation
1 2 Next

Robots with Wheels

21 posts
dubbie

RoboBobLet#3

Posted by dubbie Apr 2, 2018
Robots with Wheels Enter Your Electronics & Design Project for Your Chance to Win a $100 Shopping Cart! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   I thought I would try and measure the speed of the continuous servo motors so see how this varied with the servo setting. I am using the Servo.h library so the servo settings are between 0 and 180. For a continuous servo motor 90 is stationary. Values above 90 are direction and values below 90 are t ...
mcb1

HaloBOT

Posted by mcb1 Top Member Mar 30, 2018
Robots with Wheels Enter Your Electronics & Design Project for Your Chance to Win a $100 Shopping Cart! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   This robot was a collaboration between my daughter and I. The idea was she could use flowchart software to program it, however that never really happened.   The design was based on an earlier and slightly larger model I built. I had assisted the local school in a challenge and felt the 'feel ...
mcb1

300g BOT

Posted by mcb1 Top Member Mar 30, 2018
Robots with Wheels Enter Your Electronics & Design Project for Your Chance to Win a $100 Shopping Cart! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   This project started life as a challenge. The local Robot Club (who spend time on everything except robots) was looking to get back into robots since they had a sumo ring.   We talked about making something small and decided on the 300g class. It allowed for new and younger members to make s ...
Robots with Wheels Enter Your Electronics & Design Project for Your Chance to Win a $100 Shopping Cart! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   I decided to use a fairly common chassis from feetechrc (www.feetechrc.com) FT-MC-003 available from several distributors as it provides the four continuous rotation servo motors as well as the wheels and rubber types, plus the chassis which all fit together nicely, albeit a bit fiddly. The photogra ...
hannanrasheed

My first bots

Posted by hannanrasheed Mar 25, 2018
Robots with Wheels Enter Your Electronics & Design Project for Your Chance to Win a $100 Shopping Cart! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   My both the bots one is autonomous and another is manual they run on an arena. They are self mapping robots helps in developing automation around the malls to serve ease for packing and bringing to customers in the mall. ...
dubbie

RoboBobLet #1 : Blogging

Posted by dubbie Mar 20, 2018
Robots with Wheels Enter Your Electronics & Design Project for Your Chance to Win a $100 Shopping Cart! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   I found out where the blog happens! Major success. All I need now is to find out where the tags are. Found it! (It's only difficult when you do not know how to do it.) ...