Simple Electronic Repairs

Monthly project competitions, chances to earn prizes, you decide project themes, your ideas, your projects, turn ideas into projects.

Back to The Project14 homepage

Project14 Home
Monthly Themes
Monthly Theme Poll

 


I have an old radio ITT Schaub-Lorenz Touring International 103 which had small issue with bass control circuit. Issue was caused by "cold joint" around the potentiometer used for bass regulation.

 

Here are steps of the radio disassembly:

1. Remove the knobs from top panel.

Knobs remove.

2. Unscrew all screws from rear panel.

Rear panel.

Rear panel.

Rear panel.

Rear panel.

Rear panel.

Rear panel.

3. Unscrew all screws from top panel.

Top panel.

Rear panel.

4. Remove rear panel.

5. Unscrew two screws located near the handle.

Front panel.

6. Remove front panel. Be careful because speakers are connected with wires to main board.

Front panel.

 

Debugging part.

schematic

After short analysis of part of schematic related to tone control circuit and quick measurements of continuity I have found that issue was caused by "cold joint". There was no connection between of R334 potentiometer and C388 capacitor. The "cold joint" was marked by red square on one of following pictures.

debug

debug

debug

After re-soldering of this joint, the issue was fixed. Here is short video of disassembled radio.

 

Here is short video after issue fix.