Skip navigation

Techno Toys

9 posts
In the spirit of MakeVember I thought I would post a few things I am fooling around with. I have been working on a kit of parts and craft supplies for my granddaughter to exercise her creativity, start her on the maker path and have some fun doing it. The second video shows where I have gotten so far. The first video deals with making robot mazes and boxes. Traditionally, making a maze for a robot has been a fairly major undertaking. I wanted to find a way to make a maze in a few minutes and ...
Merry Boxes & LEDs Enter Your Project for a chance to win a Maker Tool Kit, an Oscilloscope Grand Prize for the project that brings the Most Joy to the Heart, and Gift to Gives! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   Sparky returns ..... Just a little fun and levity to say Happy New Year! Nothing like a cute new-born chick to welcome a new year...   I have been fooling around with magnetic levitation - will try to work it into a ...
I gathered up some toys and thought which one of you can be tech upped (is that a word?) and be useful to this contest.   The spikey fish and duck shouted pick me. Oh it will be another day for you. I had to go with the LED duck we brought at some Dollar Store a long time ago for $3:00. Can the LED lights work with the Raspberry Pi NoIR Camera Board and see in the dark. I have  one but really never put it to the test. I am using the Raspberry Pi 3 but really any Pi or LED Duck shoul ...
This entry in the Project14 Techno Toys competition is mainly to boost participation without setting the bar too high. I don't have a lot of toys around the house that I own, but I did find one that nobody laid a claim on. I call her Sparky. In this project I am taking a little wind-up hopping toy (Sparky) and retrofitting an LED powered by a power-scavenging circuit. The power-scavenging transducer is a piezo disk mounted under Sparky's feet, so when she hops, the disk gets flexed and gener ...
Molham

DollaS Dancer

Posted by Molham Apr 30, 2017
DollaS Dancer   Introduction: My girlfriend came up with this crazy idea! Turning a barbie into a dancer on a stage, The stage is coin bank, so you have to put money into it to make it dance for you.   Figure (0): Barbie Toy   Description:   BOM: 0. Barbie with swimming suit. 1. Right Angle Gear Motor: voltage is 4.5-6V with a no load current of 190mA, output shaft is 9mm long and the gearbox ratio is 48:1 with a wheel speed of 140 RPM (unloaded)2. Dual Ball Bearing H ...
My little daughter threw away this toy and it just stopped working. I had two options: 1. Find the bug and fix it 2. Replace the whole inside with cool stufff.   This is the room i have inside: Originally the toy came with 1 motor. There is enough room for two dc motors. Also i have arduino nano and a bluetooth receiver. The remote control can be my phone, or  i have ps4 remote which is also bt. I just need to figure out if it can be connected to arduino.   Update 1: I h ...
tech_nut81

Xylophonomatic

Posted by tech_nut81 Apr 21, 2017
So, if you've seen my comment on "Give New Life to Old Toys by Turning Them Into Techno Toys! ", then you know I'm trying to turn my old Fisher Price, pull-a-tune xylophone into an object avoiding, robot xylophone. I took the advice of the people that replied to my idea and built an auto avoidance prototype first. I used one of my sons old remote control trucks that no longer worked by remote control. Here is a picture of my prototype. (I'll try and upload some videos a little later). Fo ...
rsc

Bob_007

Posted by rsc Apr 18, 2017
I think this little guy - let's call him Bob, needs a makeover....... Stay tuned.... First we disassemble Jonny-5 Then we make a bracket for the "attachment" and......Bob_007 is complete! Bob is a bit heavy for the mechanism, so he had to loose some girth Once I get him balanced, he should fly well. Enjoy, that's my Project 14 entry for this month....... Scott ...
Project14 Monthly project competitions, chances to win prizes, you decide monthly themes, your ideas, your projects, turn ideas into projects. Back to The Project14 homepage About Project14 Theme Archive Monthly Theme Poll   This poll is now closed.  You voted for Going Green and it will launch on June 14, 2017!      Please visit Project14 | You Decide the Next Monthly Project Competition! to continue the conversation and vote on the next project competition. &# ...