Skip navigation

Techno Toys

1 Post authored by: idanre1
My little daughter threw away this toy and it just stopped working. I had two options: 1. Find the bug and fix it 2. Replace the whole inside with cool stufff.   This is the room i have inside: Originally the toy came with 1 motor. There is enough room for two dc motors. Also i have arduino nano and a bluetooth receiver. The remote control can be my phone, or  i have ps4 remote which is also bt. I just need to figure out if it can be connected to arduino.   Update 1: I h ...