Skip navigation

The Holiday Special

December 2017 Previous month
So, I have completed my DIY FLiP Connected X-Mas Ornament and displayed it on the old X-Mas tree.  It all seems to be working fine and I even added the option to dim certain colors.  Also, I created a case to house the FLiP, OLED and Bluetooth module and added some extra pieces to the case to give it a bit of a Steam Punk look.   Image of the board I put together for the Parallax FLiP circuit Parallax FLiP, OLED, and Bluetooth modules connected to fron panel:   RGB M ...
RichSr40

Merry Christmas

Posted by RichSr40 Dec 28, 2017
Hoping everyone had a great Christmas, and a fantastic year! ...
The Holiday Special Enter Your Project for a chance to win $100 Shopping Carts, Gifts to Give, and a 3D Printer Prize! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll       For the Holiday Special Challenge, I decided to make a Clausometer, as seen in the movie Elf.   As you may recall, Santa's sleigh had trouble flying due to a lack of Christmas spirit. The sleigh was equipped with a Clausometer that indicated the level of Christmas spir ...
Just a little side project with the Adafruit Pi OLED Display. It's a very tiny (26mm x 8mm) OLED Display.   On this little display I have created a Holiday Greeting by modifying one of the included python examples provided by Adafruit.   Thanks for stopping by this post.   Happy Holidays   Trent ...
This is an update to my FLiP Connect X-Mas Ornament project.  For this update I have added a second RGB board for a second Ornament, added a Parallax 96x64 OLED Display Module for a Snowman graphic, and configured Flask on a Raspberry Pi to control the RGB colors remotely from a Browser.   One of the unique features of the Parallax Propeller Processor that is on the FLiP is that has what Parallax calls multiple Cogs.  This is sort of like multicores, but each Cog is a bit more i ...
wolfstarone

3D Printer using Pie

Posted by wolfstarone Dec 20, 2017
Would like to see a 3d printer being ran by a Rasberry Pi ...
The Holiday Special Enter Your Project for a chance to win $100 Shopping Carts, Gifts to Give, and a 3D Printer Prize! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   FLiP Connected X-Mas Ornament  Hi,   Here is an X-Mas project I have been working on.  This is a Bluetooth connected Ornament that uses a Parallax FLiP board, WS2812B RGB LED Module and a Velleman HC-05 to control the color displayed in the Ornament.  The Ornament was ...
The Holiday Special Enter Your Project for a chance to win $100 Shopping Carts, Gifts to Give, and a 3D Printer Prize! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll     Introducing the Infinity Living Christmas Wreath. This was created by my kids Chrystal, Nicholas and myself. We wanted to create something for the season that would be unique. So here it is.   What we used to create the wreath:   Christmas wreath 144 RGB LED light st ...
The Holiday Special Enter Your Project for a chance to win $100 Shopping Carts, Gifts to Give, and a 3D Printer Prize! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll     Project Elf House Complete!   I would like to submit my project for both The Holiday Special and Cool LED Display contests.   If I was lucky enough to win the 3D printer I would use it to produce the casing for my Reci-Pi, my submission for Design Challenges P chef d ...