Skip navigation
Vision Thing Enter Your Project for a chance to win an Oscilloscope Grand Prize Package for the Most Creative Vision Thing Project! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   Overview Hardware Framework Collecting Dataset Image Labeling Training Implementation Testing Conclusion Overview My project idea is to used the BeagleBone AI board + Mini Power Bank + USB camera to make a Portable Dried Sea Cucumber Spec ...
Vision Thing Enter Your Project for a chance to win an Oscilloscope Grand Prize Package for the Most Creative Vision Thing Project! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   So its been a little bit since I got the beaglebone_ai so I thought I would finally do a post on what I have been working on.  So it all starts out of necessity when it comes to projects for me so with the bb:ai there was certainly a ton of things I could have done with ...
Introduction  Law enforcement officers are often searching for vehicles that have been reported stolen, are suspected of being involved in criminal or terrorist activities, are owned by persons who are wanted by authorities, have failed to pay parking violations or maintain current vehicle license registration or insurance, or any of a number of other legitimate reasons. Victims and witnesses are frequently able to provide police with a description of a suspect vehicle, including in some c ...
Vision Thing Enter Your Project for a chance to win an Oscilloscope Grand Prize Package for the Most Creative Vision Thing Project! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   Poop Buster Setup Beaglebone AI is used to control a x-y gantry robot by controlling it via USB serial port. some videos are attached towards the later part of this blog   My Journey I initially struggle with the insufficient disk space on my Beaglebone AI but solve ...
Vision Thing Enter Your Project for a chance to win an Oscilloscope Grand Prize Package for the Most Creative Vision Thing Project! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   IdeaThis project is an attempt to build a in-car safety device, which monitors drivers' attention to the road and create alerts if the driver becomes sleepy or distracted. The statistics are quite alarming in regard to drowsy driving. Here are some numbers from the US  ht ...
dixonselvan

The Watching Picture

Posted by dixonselvan Top Member Nov 18, 2019
Introduction        While thinking about doing a project for Halloween, this idea popped up in my mind. Imagine you are staring at a picture and looking at the details. Suddenly if the picture turns scary! As shown in the animated image below?  Who will not be scared to their bones? Source: https://images.app.goo.gl
KLtCh9qfa8S8MzB9   What does this have to do with Vision Thing - Project14 competition?        The above idea wil ...
Vision Thing Enter Your Project for a chance to win an Oscilloscope Grand Prize Package for the Most Creative Vision Thing Project! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   1. Introduction 2. Idea 3. Build Lamp Mounting the RGB LED strips RGB Controller Camera Mount Medication Organizer 4. OpenCV 1. Introduction     Hi! This will be my entry for the Vision thing Project14.  I wanted to ...
Vision Thing Enter Your Project for a chance to win an Oscilloscope Grand Prize Package for the Most Creative Vision Thing Project! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   Smart Security Camera (with attendance on Google Sheets)  Summary The AIM of the project is to make a smart camera that can monitor your house, office, etc and give you valuable data like keeping track of who is on the door, at when did any person arrive, click photograp ...
OK, so now  I have gotten the BB AI up with its output on my tv. I have plugged in a Dell keyboard with a mouse into it as well. My ethernet cable is plugged in and active. I got a good deal for an Optrex 4x20 which has a ribbon cable attached to it. So I'm going to break out my Metcal and unsolder the ribbon cable, and then replace it with a 16 pin header into which I will plug I2C driver directly into the header. I think I will be limited on what I can see as I only have my webcam (USB) a ...
TABLE OF CONTENTS INTRODUCTION BBAI SETUP CHECKLIST GOOD STUFF TO KNOW PINMUXING Pinmux Procedure a BBAI compatible dts file ANALOG INPUT sys file pin mapping I2C USE PWM CONTROL AUDIO CREATING A RAM DISK TRANSFERRING FILES TO AND FROM OTHER MACHINES Cloud 9 Upload Feature GitHub wget Windows Shared Directory CODE EXAMPLES Augmented blinkLED.js classification.cpp analogIn.c i2cLCD.c tfmini.c pwmout.c ...
Vision Thing Enter Your Project for a chance to win an Oscilloscope Grand Prize Package for the Most Creative Vision Thing Project! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   Content Content 1. Introduction 2. Codes 2.1 Versatile Inter Processor Connection, Remote Connection and PinMux 3 Hardware and Build 4 The AI Lock, Finally Reference, Forget your KEY and your SECRET PASSCODE? That is OK if you are with AILOCK. & ...
I wanted to make a terminal connection to the BeagleBone AI board I have, just to make sure I could still do things if I messed up elsewhere - which is something I have done with other boards. I am using a FTDI232 board to make the connection to the BBAI terminal connector. As I was buying one of these boards for the BBAI I decided to buy one as part of a package with an ESP32 CAM and some Dupont cables for later fun.   I was able to obtain a suitable cable (thanks shabaz ) that connects t ...
Vision Thing Enter Your Project for a chance to win an Oscilloscope Grand Prize Package for the Most Creative Vision Thing Project! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   The Artificial Neural Network that I want to use with the LDR camera and the BeagleBone AI is one derived from a book by H Pao. As it has been some time since I used this programme I thought it would be beneficial to refresh my memory of how it works. Fortunately I have a cop ...
I am trying to find a connector and wires for the 3 pin TTL serial connector on the BeagleBone AI. I know that it is 1.27 mm spacing but I have not been able to locate anyone who can sell me a connector with wires and connector. I have purchased a FTDI USB to serial convertor with 0.1 inch spaced pins for Dupont connecting wires so I just need to convert from 1.27 mm to 0.1 inches (2.54 mm). I know they exist, I just cannot find any.   I can remember reading about this in a comment on one ...
Vision Thing Enter Your Project for a chance to win an Oscilloscope Grand Prize Package for the Most Creative Vision Thing Project! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   As I cannot think of any more excuses for not powering up the BeagleBone AI so that I can use it to run the ANN for my LDR Camera, I decided to try and get it going. I thought I had a Raspberry Pi 3 power supply that came with a Type C connector but as it turns out, I haven't ...
Vision Thing Enter Your Project for a chance to win an Oscilloscope Grand Prize Package for the Most Creative Vision Thing Project! Back to The Project14 homepage Project14 Home Monthly Themes Monthly Theme Poll   What started out as a jokey discussion between some Element14 members ended up with an interview, talk and webcast, and nearly won me $5000 My initial entry was as follows: This remarkably got me into the competition so they sent me a DragonBoard.   The first step ...