Hey yall, I made a very inexpensive development box for my new Raspberry pi using 5 to 24 spaces organizer box I bought on Home depo and some buttons and battery holder so now my Rpi works on batteries prety cool.

 

Soon Ill be uploading a video of it explaining the use and the final demonstration.

 

The box is not yet ready because I need to install the GPIO port and connect the 5V fan to the Rpi for cooling but I tested it using and xbox intec 7" lcd screen and I have yet to run out of battery due to the los power the Rpi utilizes, its very cool to work with the Rpi and when I guet it to link up with my arduino its going to be cooler, it allmost looks like a laptop from the side.