Skip navigation
In Participation of Element 14s Awesome Global Arcade project bkutzsch and myself will team up as Team "K", AKA KillerByte.  :-)   I am in the process of getting an old school full size arcade system to be the body for this project.  I know spannerspencer specified we didn't have to work an old school cabinet in but when I came across one and then that very night read about this awesome offering by Element 14 it seems as if this is meant to be.  Right now there are two poten ...
dannyr

Gameboypi

Posted by dannyr Mar 19, 2016
Currently working on a GameBoy Pi build and ran into a small snag need somebody that can help me figure out some minor wiring issues   Wiring help on a Gameboy pi project. ...
Raspberry Pi is a great component for building low cost servers!As reported yesterday on the Raspberry Pi Blog, Mythic Beasts managed the online launch of Raspberry Pi 3 in part by hosting it on Raspberry Pi itself ! It was an impressive example of eating your own dog food and Raspberry Pi 3 rose to the challenge for quite a while. Check out Raspberry Pi's latest blog to learn all the details but suffice to say we think Raspberry Pi 2 and now Pi 3 are an excellent choice for building servers. Li ...
Cost effective industrial computing in a familiar form factorIt's hard to spot the difference just looking at it but the new Raspberry Pi 3 pictured above with its predecessors is the latest iteration of Raspberry Pi in the popular "Model B" form factor and it's a cracker ! Our friends at Raspberry Pi and element14 gave us samples and invited us to exhibit BitScope Blade at the Raspberry Pi 3 launch held today at the Shard in London. Eben introduced this new model to the world as we celebrated ...
I recently had the opportunity to take the Raspberry Pi 3 Model B out for a test drive.   The form factor of the new Raspberry PI is the same with the exception of the LED’s being moved from the right side to the left side of the board (Pi facing up with USB data ports facing you).   If you have a clear case or you don’t mind having your view of the LED’s blocked then most cases that fit the Model B+ or the Pi 2 model B will fit the Pi 3.     I ...
With our ever increasing media libraries containing movies, TV shows, music and pictures we need something that can serve this content to any of our devices.    If you fancy opera in the kitchen, jazz in the bathroom and the latest Hollywood blockbuster in your pocket, then you need a media server and the Raspberry Pi 2 is the ideal low cost candidate. To replicate this project you will need:   A Raspberry Pi 2 A laptop running Windows/Mac or Linux A minimum of 8GB SD card ...
Thanks to Gareth Halfacree, whom took a series of photographs of the Raspberry Pi processor under heavy load, I think. Note there's no load on the GPU in these photographs. You can see how potentially hot each processor chip of the Raspberry Pi get. These are at stock processing speeds with no overclock and using sysbench to push the CPU.   element14 does sell Raspberry Pi Heatsinks   Raspberry Pi Operating Temperatures Normalised Scale Raspberry Pi 1 Model A+: Normalised Temperat ...

Filter Blog

By date: By tag: