Skip navigation
OVERVIEWIn this article we'll show how to control your Raspberry Pi terminal from Facebook.   Below is a block diagram illustrating how we set up a web application running on a Raspberry Pi, made available to a Facebook application webhook via dataplicity Wormhole. PREREQUISITESYou will need: Raspberry Pi connected to the internet. Dataplicity installed. If you need some help to get up to speed, see Getting started with Dataplicity. CREATE A FACEBOOK ACCOUNTThis will be the administ ...
I found this distribution to be the simplest to install, localize, and set-up networking for (wired or WiFi, static IP or DHCP).  I was impressed enough that it is on all of my computers: RPi2 (ARMv7) SoC Pine64+/2GB (64-bit ARMv8, like RPi3) SoC Biostar NM70I-1037U (Dual-core 1.8GHz x64 Celeron) motherboard Zotac IONITX-FE (Dual-core x64Atom 1.6GHz) motherboard   I am using version 16.04.  The only major flaw (WiFi not processed during installation, https://bugs.launchpad.ne ...
This is a much-needed update to the blog entry that I wrote in April 2015 with respect to RPi2 and was last updated this past September.  Much thanks for comments by clem57 , anthonyworth , and sergiokob (RPi3 comments). Why a static IP address for the Pi?  Well, you might not want it to change so that you can use a Pi in the following example repeated situations: sshd (allow ssh clients to connect for various reasons) rsync (copy from/to over SSH) remmina (remote desktop server) ...
  This is a much-needed update to the blog entry that I wrote in May 2015.  Thanks to subsequent comments by Daniel Carrion (off, busy on other things now), Jose Berrios, kiltedken , suprimex , dirkbroer , and mchuntley.   In September 2016, the current Raspbian boinc-* packages will, indeed, get you a working boinc project on the Raspberry Pi 2 - just avoid installing the boinc-app-seti package from Jessie.  Yes, this blog entry is smaller because one year's progress has s ...
  This video is all about connecting MCP3208 with Raspberry Pi and accessing it using JAVA. ---------------------------------------------------------------------- Repository : https://goo.gl/7NRe5n Schematic : https://goo.gl/kbkhj4 Code : https://goo.gl/J0BT8p Compiled JAVA App: https://goo.gl/pvb6Sp Lib :  https://goo.gl/NyI9vL   ---------------------------------------------------------------------- Subscribe : http://goo.gl/gM134X   Guys Subscribe to my chan ...
  This week, the Raspberry Pi foundation celebrates another milestone with the announcement that they have sold over 10 million Raspberry Pi's around the world.   As a leading distributor and manufacturer of the boards, Premier Farnell has manufactured and sold almost seven million devices, not to mention millions of accessories and related products. Our element14 community has also become one of the leading platforms for Raspberry Pi enthusiasts, with thousands of members sharing th ...

Filter Blog

By date: By tag: