Skip navigation
2016
I'm a PI 3 newby and I want to replace my Media Center which is a matricom q unit. Would this be better? ...
NEW! Raspberry Pi 3 Model B Frequently Asked Questions Comparison Chart Technical Specifications 40 Pin Out Pi3 Video Arcade Project   Our good friend biglesp put the Raspberry Pi 2 to the test the last time around, though I feel that he missed a good number of possible benchmarks to run on the hardware. With that in mind, I'm going to test the main boards of the Raspberry Pi that I can get my hands on and not only run the main benchmarks Les ran, but also a good few more thanks to Roy L ...
This blog tutorial will address taking advantage of features available in X Windows on the Raspberry Pi.   What is X Windows     From Wikipedia: The X Window System (X11, or shortened to simply X, and sometimes informally X-Windows) is a windowing system for bitmap displays, common on UNIX-like computer operating systems. X provides the basic framework for a GUI environment: drawing and moving windows on the display device and interacting with a mouse and keyboard. X does not m ...
http://www.pcworld.com/article/3027446/hardware/irate-comcast-subscriber-turns-raspberry-pi-into-a-watchdog-for-slow-internet-speeds.html   One Comcast customer has a Raspberry Pi complain to the company every time his fast connection becomes too slow.  Ian Paul | @ianpaul  Contributor, PCWorld Feb 1, 2016 8:34 AM There’s nothing more frustrating than dealing with slow Internet at home, especially when you’re paying a steep premium for a fast connection speed. Wash ...

Filter Blog

By date: By tag: