Skip navigation
Raspberry Pi have (today) launched the new Raspberry Pi Zero Wireless.     For more information on the Raspberry Pi Zero range, including where to buy the new Raspberry Pi Zero Wireless please visit the Raspberry Pi Foundation website at https://www.raspberrypi.org/   Happy 5th Birthday Raspberry Pi! ...
Hello Again, As i said in others post of mine i am working on a house automation system based on raspberry pi and arduino ... I ve moved a lot with this.. I also writing a program for this. I wrote the program in Visual basic 2010...it has over 1000 lines of code cause it is also like JARVIS from ironman... It can execute a dissent amount of pre installed commands. I also added a feture when the doorbell ring a window pop up in my screen and it show me who is in the front door with face recogn ...
Almost everyone has heard of RetroPie.     The open source software which has enabled a bunch of Ikea tables with embedded Raspberry Pi.   Unfortunately, they've recently learnt a bitter lesson in trademarks, that unless you get there first, someone else can pull the rug out from under your feet, as the makers behind RetroPie call out for legal help.     Amazingly, someone from India has setup a website selling Raspberry Pi's with the software on the SDCards, some ...
A few months back, I enrolled for a design contest at hackster.io . Needless to say its one of those contest where hundreds(500) of people join but every few complete. Anyway I did my part and here are a few tit-bits I gathered.   The implementation I initially though about adding a massive array of features but then remembered that it was a contest sponsored by Cypress. Instead I worked on one part and ended up getting stuck in a loop. I started with the Texas Instruments MSP430 and fina ...
Not even a near record breaking heatwave can stop BitScope Blade hosted Raspberry Pi servers as we discovered by accident when our trusty old Dells came to an ignominious end but the 32 BitScope Blade Raspberry Pi in the same overheating room survived without skipping a beat!   We had an unexpected demonstration of just how robust Raspberry Pi is as a compute platform this week. If you live downunder where our R&D headquarters are, you will know it's been very hot for quite a while. It ...
Following the recent launch of BitScope Blade and the case studies about the weather station in Nepal and the interactive Theremin exhibit at MAAS we received a lot of questions about which Blade is best for what purpose. Read on to learn why Blade comes in three editions and how you can best make use of them.   BitScope Blade Reloaded is our computing infrastructure platform for Raspberry Pi.   It is available in three editions; Uno, Duo and Quattro which power and mount one, two or ...
Hi,   I want to introduce a new small project of me. It's a OLED display shield for Arduino and Raspberry Pi. The shield includes 3 buttons and leds to realize simple menues etc. The communication with the Arduino or RPi works via I2c. You will need only 4 wires to connect the shield.   Pls check this link for sample code and more information   The pcb fits perfect in our DIN rail enclosure sets for Raspberry Pi and Arduino.     ...

Filter Blog

By date: By tag: