Skip navigation
The Raspberry Pi 4 can easily be configured as a 2.4 GHz or 5GHz routed wireless access point or as a bridged wireless access point.   My intention was to create a wireless network outside of the home. The configuration only took a few moments thanks to resources provided by @raspberrypi.     The results are excellent. Speed and signal strength are more than expected. Good enough for flawless hd video streaming and quick downloads.     Cheers to Raspberry Pi!! &# ...
Introduction The Monarch Go Pi HAT is a cellular connectivity add-on card for SBC boards that have a Raspberry Pi HAT-compatible connector. Fitted with Sequans Monarch Go (or Monarch Go GPS) LTE Cat-M1 modem, this HAT board also facilitates expansion via Click boards using a compact onboard Click Shuttle connector. Noteworthy is that an integrated onboard USB-UART bridge interface allows this LTE HAT to also be used with other platforms.   Version Date Version Revision 18 June 20 01 Initi ...

Filter Blog

By date: By tag: