Skip navigation

Raspberry Pi

7 Posts authored by: balearicdynamics Top Member
More than a news it is an announcement.  Maybe not so much time has passed by the end of the Pi Casso Challenge and some members still remember the Art-a-Tronic project and Seven of Nine, the Borg. Almost one year after the project started today I start officially the Art-a-Tronic web site and blog in the self-explaining domain name   we-are-borg.com  On the website, you will find all the episodes of the Art-a-Tronic project and exhibition in videos, as well as a blog with the f ...
A Pi-Day News I hope will be appreciated(by all the Italian language users of the community)  Today, 3,14 2020 I am proud to announce that the new book "Progetti per Maker con Raspberry Pi" has been passed for the press to my publisher Ulrico Hoepli. The book will be available soon on the Italian libraries and on Amazon. The book includes many Raspberry Pi projects into the first part along a path from easy to complex: the Pi Scope, Pi Cade, Pi Vision, Pi Rotary, Pi Cluster. The second ...
Introduction Platform scenario Building the structure Wooden frame Fixing the mirror Assembling the mirror back side Keeping the LCD in place Adding the Raspberry Pi and wiring all together Raspberry Pi Cooling Adding the Pi devices Fixing the back layers firmly Last touch: positioning the camera Finished setup and some anticipations Introduction Having to develop a MagicMirror project almost flexible to fit in different contexts including extr ...
I decided to write this post due a silly trap that to be honest I think should be avoided in next updated of the raspbian pixel version. The last official downloadable version at the date is the 2016-11-25-raspbian-jessie.img   Here and there there are tons of posts of users that are not able to connect via SSH to a fresh raspbain installation on a PI3 of this version; I had the same problem too and tried to solve the problem thinking to the most common issues like removing the .ssh/known_ ...
This is not a problem but a fact. And there is also a precise reason: the first model of the PI, with 256 Mb ram uses the I2C channel 0 instead of the I2C channel 1 adopted in the further versions. So, as the Microstack accelerometers is hardware compatible with the PI model A+, the software no.   The key was to discover from what was depending this issue, that is the i2C channel settings. And nothing changes if you manually enable also the channel 1 because it is question of internal sett ...
I suppose that it is not rare that tying for a solution the approach will be installing packages on the Raspberry PI environment, check how the stuff works then abandoning the solution to move to a different approach. This usually means sudo apt-get install a certain number of packages and the related dependencies occupying storage space.   Deciding that a certain approach is not what we want we can remove the packages in the same way se installed them: $> sudo apt-get remove <pac ...
There is something that I use almost intensively on the Linux environments and after testing this feature on Pi SSH connection I have decided to make this post. Frankly I am not sure if I have find nothing about the -Y feature mentioned around Element14 because it's so obvious to be silly or it is really a very few used feature. Apologise if it is the first case   This feature has been tested with raspian wheezy on all the Raspberry PI models included the first version no more available on ...

Filter Blog

By date: By tag: