Skip navigation

Raspberry Pi

12 Posts authored by: gam3t3ch
  So over the past while I have done a lot of things with the Raspberry Pi.  Sure I use the Raspberry Pi 4 as a desktop daily and read books on Raspberry Pi and enjoy looking at everyone's projects cause there is just too many amazing things being created with the Raspberry Pi.  I tip my Rpi to you to those that make and use it.   I felt like it was a good time since I even recently am in a roadtest for the raspberry pi, to review all the fun I have shared so far on the co ...
  I have been recently selected for a roadtest on element14.com the Raspberry Pi 3 in a box. This is the official Raspberry pi kit which includes tons of goodies but I need information from you first! I am following my guidelines that I setup for this roadtest this is why I was selected so please feel free to follow along and join in this will be my first interactive roadtest and I think the first of its kind on the element14 community roadtests.   You can check out more on the road ...
  I will say there was a lot more in depth information at the course a bunch more fun as we even had samreen.islam on a google hangout showing off a project once again thank you to matrixlabs for being apart of the course.  I will say there was a bunch of Minecraft in there as well.   This is part 1 I will certainly be putting more materials together and bringing more video's on the raspberrypi soon.  I hope you enjoy the video and to anyone new to Raspberry Pi all the ...
#Open Terminal Press Ctrl + Alt + t on your keyboard #install PCI utilities sudo apt-get install pciutils #run on every boot sudo nano /etc/rc.local #add the command before exit 0 sudo setpci -s 01:00.0 0xD4.B=0x41 #reboot sudo reboot     ...
So I have been meaning to do an update and found this and its great for anyone not wanting to do it the other method that I had posted about setting up your SSD as a boot drive on the Raspberry Pi 4 check it  out.     You can download the Berryboot files here: https://www.berryterminal.com/doku.php/berryboot   To install: extract the contents of the .zip file to a normal (FAT formatted) SD card, and put it in your Raspberry Pi. This can be simply done under Windows witho ...
    So if you plan on using your Raspberry Pi 4 as a desktop or any other Raspberry Pi.  One thing I cant stress enough if protection if you have a web browser in use and your online you want to make sure that you have some sort of protect and a good starting point is with some Malware and Antivirus protection.   Now from my understanding LMD (Linux Malware Detect) will run with clamav now is it working 100% with clamtk?  it seems to be but I could be mistaken scans do ...
  You can either check out the video above or check the info below or both!   So this morning I decided I would update my raspberry pi.  seems there was a ton of firmware updates that needed to be installed in the new update so onward and forward I went with the sudo apt-get update && sudo apt-get upgrade at first this was great  when it was finished everything was still working fine.  Then came the reboot on the system...uhoh  no mouse no nothing going ...
    So previously, I had wrote a post about my experiences with using the previous versions of the Raspberry Pi as a desktop with multiple version and I enjoyed them as a great addition to using them along side my main PC.  Since I was unable to do all the things on previous versions I was hoping to do with the Raspberry Pi I had to settle for just being able to do most things.   Now knowing what was and wasn't working on previous versions of the Raspberry Pi I finally got ...
  **Small update: [Oct.13.19] Remember to also plug your audio into another speaker system as well.  Today I thought I had this issue again so  I ran the fix and was getting frustrated that it wasn't working.  Turns out that my speakers on my old monitor that I am using finally went and now I have to find a low powered replacement so remember to also try hardware as well to make sure it is working (I could have run my phone into the monitor to test it which I eventually did ...
Once you play around with all the IDE's available for python on Raspberry Pi you tend to want to play with PyCharm since well its probably what you have installed on your desktop or laptop.  Good news get it up and running on the pi in no time.   This is one of my favorite ones but tend to use MU IDE on smaller projects.   Go to https://www.jetbrains.com/pycharm/download/ download the linux community version in the downloads folder on your pi extract the files by right cli ...
See quite a few tutorials on hooking up a hard drive to the pi for and just want to give my quick and easy version cause I tried a few and they didn't work.     install buster on sd card :  https://www.raspberrypi.org/downloads/   insert into your pi and boot up do the first time setup and updates.   plug in your ssd drive   go to the pi menu and then to accessories click on SD Card copier   copy from device:  your SD Card copy to device:  ...
I am currently running this on a Raspberry Pi 2 with Debian "Raspbian GNU/Linux 9 (stretch)"   1. sudo apt-get update 2. sudo apt-get install apache2 3. sudo mkdir -p /var/www/yourdomain.com/public_html 4. sudo chown -R $USER:$USER /var/www/yourdomain.com/public_html 5. sudo chmod -R 755 /var/www 6. nano /var/www/yourdomain.com/public_html/index.html   ----------------Add the following to the index.html file------------- <html>   <head>     < ...

Filter Blog

By date: By tag: