• Enrolling RoadTests: 1 week to go for the Raspberry Pi HQ Camera

    There's one more week to go for enrolling in the Raspberry Pi High Quality Camera Roadtest.   You can submit an application by going here: https://www.element14.com/community/create-roadTestApp!input.jspa?contai...
    Profile Photo
    created by rscasny
  • Why do the specs for the PiB not include a mechanical -  for mounting hole distances?

    Can anyone provide since Element14 seems unwilling -  do they want us to use these or not?
    Profile Photo
    last modified by sharktank72
  • Raspberry Pi 3 Model B Unboxing - Official element14 Video

    NEW! Raspberry Pi 3 Model B Frequently Asked Questions Comparison Chart Technical Specifications 40 Pin Out Pi3 Video Arcade Project   Here's your first peak at the brand new Raspberry Pi 3 - the fastest Pi ev...
    Profile Photo
    last modified by pchan
  • Find element14's Five Hidden Raspberry Pi 3's

    NEW! Raspberry Pi 3 Model B Frequently Asked Questions Comparison Chart Technical Specifications 40 Pin Out Pi3 Video Arcade Project   The Raspberry Pi 3 is out now, and setting the cash registers on fire, it'...
    Profile Photo
    last modified by pchan
  • Raspberry pi 3 No audio through HDMI

    I need some help fixing the audio so it comes out through the HDMI cable. Also how do I reboot?
    Profile Photo
    last modified by cowboytanaka88
  • Omnibot Michelle--Ultrasonic sensors

    So during this quarantine period I began working on a pet project to make a robot companion. I didn't wish for it to be WiFi or keyboard controlled--fully autonomous and able to navigate for itself. So far I have been...
    Profile Photo
    created by ajkatz83
  • Raspberry PI 3 ACL Ligth is not blinking y stay off

    Hi to all, Please girls and guys, i need help to test my Rapberry PI 3 Model B+. When i put the energy cable on the RaspberryPI using differents SD Cards i have no boot of this device, the screen stay in black and th...
    Profile Photo
    created by caromeva
  • Pi Desktop: max current output?

    Hello   I have purchased a Element14 Pi Desktop that I'm using with my Pi 3B+ and the original Raspberry 2.5A PSU. So far it was running fine with the RTC hat + SSD + 2 fans on the GPIO (1 for the heatsink and...
    Profile Photo
    last modified by rootard
  • Error when running winforms app on raspberry pi 3b+

    Hi,   I have a project of creating a learning-based UI on raspberry pi showing the function of a buck converter. I had created the .cs file successfully without any error on my windows laptop that can display th...
    Profile Photo
    last modified by lhj1997
  • Raspberry Pi 3 in a Box

      Tab Label Tab Content About The RPI3-INABOX-KIT features a third generation Raspberry Pi 3 Model B. It includes a lot of accessories plus an Adventures in Raspberry Pi "Foundation Edition" book to make your e...
    Profile Photo
    created by rscasny
  • Pi Desktop very disappointing

    I had high hopes for this but it doesn't appear to be very good.  The build quality seems fine and it looks good - just a shame it doesn't actually work.  Or doesn't actually work yet.   The instructio...
    Profile Photo
    last modified by masterplumber
  • GraspIO and Camera ov5647 v1.3

    I have connected a ov5647 v 1.3 camera to a Pi 3 B+.  Using GraspIO, I try to take a snapshot.  The camera turns on but it won’t turn off.  Any ideas?
    Profile Photo
    created by charlesboudreau
  • boot from ssd in pi desktop

    I couldnt find the file pidesktop.deb. The webpage is really complicated.
    Profile Photo
    last modified by gdenicolas
  • Transfer Image from Raspberry Pi (Python) to Android app (Java)

    Hi everyone! I need help transferring an image via TCP from a python program on my raspberry pi to an android application.   I have set up a client-server architecture such that my raspberry pi 3 records audio,...
    Profile Photo
    last modified by programmer.3
  • Use Raspberry Pi 3 to Control Xbox Controller

    Hello,   I received my Raspberry Pi 3 as a Christmas gift, and I was curious if I could use my device to control my controller to do actions in-game, and If there is a way to that, I would like to know how too....
    Profile Photo
    created by gameless
  • Amber Pi Design Kit

    Sign Up For the Webinar: Wireless IoT for Everyone with the Amber Pi       Tab Label Tab Content About The AMBER PI is an expansion board that equips the Raspberry Pi with the sub-1-GHz RF interface p...
    Profile Photo
    created by pchan
  • Is there a way i can connect my speakers to the raspberry pi 3 with the 3.5 mm jack? i dont get any sound when i plug them in

    Is there a way i can connect my speakers to the raspberry pi 3 with the 3.5 mm jack? i dont get any sound when i plug them in
    Profile Photo
    last modified by neeraj23
  • Raspberry Pi 3 Model B GPIO 40 Pin Block Pinout

    global.access.content.type.-NEW! Raspberry Pi 3 Model B Frequently Asked Questions Comparison Chart Technical Specifications Unboxing Video Pi3 Video Arcade Project      Graphic showing the GPIO pin breakout on the Raspberry Pi 3 Model B. &...
    Profile Photo
    last modified by Christopher Stanton
  • usb usb1-port1: disabled by hub (EMI?), re-enabling

          ---Setup---     1) We are evaluating using Raspberry Pi Compute Module CM3. 2) USB-HUB and USB-UART are boarded on the IO board. 3) USB-HUB is working in Self-power mode. 4) VBUS-d...
    Profile Photo
    created by praveendeshmane
  • Pi Desktop: mSATA disk not recognized

    Hello I hope a Rasperry Pi guru or someone @ Element14 will be able to help me:   I just bought a brand new Pi Desktop case + Hat and swapped my fully functioning 3B+ Pi and mSATA disk into it, powered on and.....
    Profile Photo
    last modified by rootard