See my original blog here Raspberry Pi car computer | Flamelily I.T


I have always loved those old TV series with futuristic tech in those futuristic vehicles, like Knight Rider, Air Wolf, Street Hawk etc. So it got me thinking about how easy it would be to add a computer to a vehicle. Now I know its been done before and a quick Google search shows multiple websites and companies making very complex car and other vehicle computers, but at a large cost.

carcomputer.jpg

Well I thought my Raspberry Pi is the perfect device for this.

  • Its cheap
  • its very small
  • small power requirements (runs off a micro USB car charger)
  • flexible video and audio outputs (HDMI and Composite RCA for video, HDMI and 3.5mm audio jack for audio)
  • and best of all you can change operating systems by simply switching out SD cards

 

Below is a photo of the Raspberry Pi running the excellent media centre type operating system Raspbmc which is perfect for browsing and playing your media collection using a media centre remote or something similar, as shown in my ‘shopping list’ below.

carcomputer1.jpg

What I did

Well firstly I had the Xtron car DVD player for the Ford already fitted and it can be found on this site here http://www.xtrons.co.uk/ and there are DVD/Radio players for a number of car manufacturers. However you don’t actually need one of these if you can place a TFT screen elsewhere. I also have one of these..

carcomputer2.jpg

Which can be found on Ebay for about £23 at this link. http://stores.ebay.co.uk/SainSpeed This 7″ TFT can be placed in a headrest or on the dash somewhere as it comes with a stand. Both of these devices have a composite RCA video input and for audio I have a basic 3.5mm audio cable from the Raspberry Pi to the auxiliary port of the radio. So all audio is played via the car speakers which sounds really good and clear. I placed the Raspberry Pi in the centre console as shown below and routed all cables under the centre console so no cables are lying around.

carcomputer3.jpgcarcomputer4.jpg

I used the brilliant little Xenta Wireless Keyboard with mouse touchpad built-in. This works perfectly with both Raspbian and Raspbmc. It even has an on/off button on the back to save batteries when not in use (it takes 2xAA batteries).

carcomputer5.jpg

So this can now connect to any wireless network and I connect it to my mobile phone by using the portable wi-fi hotspot, giving my Raspberry Pi an internet connection even on the move (obviously don’t try browse the internet or watch videos whilst driving).

Materials Used :

  1. Raspberry Pi (Obviously)
  2. Xtrons Car DVD player
  3. 7″ TFT monitor (for back seats or main monitor)
  4. Extra composite video cable and 3.5mm audio cable
  5. Wireless N USB dongle from Amazon
  6. Xenta Wireless Mini Keyboard from Ebuyer
  7. Micro USB car charger

Update pictures of the headrest's in next blogpost here http://wp.me/p2G9uP-8j