Rapiro: Putting it together and getting it to work
Posted by Frederick Vandenbosch
Thanks to element14 and the Pi NoIR and Catch Santa Challenge, my daughter and I won a Rapiro kit with Raspberry Pi and Pi Camera.
In this post, I will describe my experiences in building and getting Rapiro up and running.
Kit
The kit came in a large white box, accompanied by a Raspberry Pi and Pi Camera.
The Rapiro kit comes in a big box which can be used later on to carry the assembled Rapiro.
All parts are neatly arranged in individual compartments.
Unfortunately, no instructions are provided with the kit.
After some searches on Rapiro's Kickstarter page and website, I was able to gather different pieces of information:
- Photo gallery on how to assemble Rapiro
- Arduino sketch for Rapiro
- Power supply recommendations
- Instructions on adding a Raspberry Pi and Pi Camera: here and here
Since Kickstarter rewards only started shipping about two to three week ago, there is not a lot of user feedback yet. Also, as I'm not a backer on Kickstarter, I am unable to post comments in order to ask questions etc ...
I've read that a discussion forum will be open soon, but until then, I'm on my own.
Assembly
Rapiro
Using the photo gallery, assembling Rapiro was easy. The photo instructions are very clear and make it very easy to compare with.
Labeling the servos and connecting them to the control board to set the initial position of the servo.
Passing the servo cables through the foreseen slots to the control board.
Connecting the RGB LEDs and attaching the final piece of the kit.
The build took approximately 2 hours and did not require any soldering, only a screwdriver and some common sense.
Raspberry Pi
It's possible to expand Rapiro's capabilities by adding different components, such as:
- Raspberry Pi and Pi Camera
- Speakers
- PSD distance sensor
These components do not come with the Rapiro Kit by default and Rapiro is able to function without them.
I installed the Raspberry Pi and Pi Camera as those were kindly provided by element14.
It's important to prepare your SD card in advance, as once the head is closed, there is no access to the SD card slot or HDMI port.
I installed the latest Raspbian, enabled camera support, wifi and ssh, in order to be able to control Rapiro remotely.
Pi and camera are installed in Rapiro's head. Pi is connected and powered via GPIO pins.
Wi-Pi connected in the back of Rapiro's head.
Testing
Arduino Sketch
The Arduino sketch for Rapiro can be modified and uploaded using the Arduino IDE and the micro USB connection.
It's very useful to update the sketch to:
- modify the initial position of the servos to properly align feet, arms, etc ... in case they weren't during installation
- program new moves
- ...
In my case for example, both feet weren't exactly sitting flat on the table and the waist was not propery aligned. So instead of taking everything apart to correct this, I modified the starting position of the feet's and waist's servos and uploaded the updated sketch.
// Fine angle adjustments (degrees)
int trim[MAXSN] = { 0, // Head yaw
-5, // Waist yaw
0, // R Sholder roll
0, // R Sholder pitch
0, // R Hand grip
0, // L Sholder roll
0, // L Sholder pitch
0, // L Hand grip
0, // R Foot yaw
10, // R Foot pitch
0, // L Foot yaw
5}; // L Foot pitch
Commands via Pi
The Arduino sketch comes with some predefined movement sequences and positions. They can be called via the serial interface of the Pi.
I installed minicom:
pi@rapiro ~ $ sudo apt-get install minicom
I couldn't find an actual list of sequences documented anywhere, so I derived some from the Arduino code.
To execute them, you pass the sequence's number via the serial interface:
pi@rapiro ~ $ echo "#M6" | sudo minicom -b 57600 -o -D /dev/ttyAMA0
Here's a little demo:
Thank you
Our cats do not necessarily like our new robot friend, but we love him!
Thank you again for this awesome prize, and stay tuned for more adventures with Rapiro.

Comments