Skip navigation
Disclaimer: I’m an engineer, not a pro film maker. Be advised.   My goal... haunted house level effects for the front door, again! If you didn't see the "Scary Door" from 2013, go see it now!   I wanted to create the sense of stifling... to overwhelm the visitor with light and rumbling sound. I figured red light would give the most horror feel with the matched sounds.   I used a Raspberry Pi B+, not on purpose, but I am glad I did. The B+ has more IO, which I took advan ...
For construction of model pictured above, 2 banks of 10 towers   Parts and Pieces (What to buy)Support Frame(5) 10' - 2" PVC pipe - See It!(1) 10' - 3" PVC pipe - See It!(4) 2" PVC 90° elbow - See It!(8) 2" PVC tee - See It!(4) 3" to 2" PVC tee - See It!(4) 3" PVC endcaps - See It!Note: All PVC pipe and fittings are Schedule 40 - cellular PVC Towers/Return(10) 10' - 2" x 3" PVC downspouts - See It!(1) 10' PVC extruded gutter 4" - See It!(4) PVC gutter end caps (make sure to get 2 left ...
It's that time of year; with spooks abound, Don't make a noise, not even a sound, As they'll find you, just you see How creepy and scary; they can be...         The Scary Door Cabe Atwell puts together an impressive feat that'll scare the pants off you. You see this door has a window, but into what? Why don't you ring the bell and find out for yourself? Or are you too scared...   Pumpkin Pi Drew Fustini decides that a pumpkin with a tea light in i ...
Hi! There is a new portable computer called Pi Vessel on Kickstarter. It's based on Raspberry. This device is for people who don't want a lot of hassle to get up and running fast. It's great for watching TV and movies without a long setup time, downloading software, putting together a console, reading instructions, or fussing about with complex cables and gadgets. The Pi Vessel is simple, affordable, and kid proof. Let's check it out! https://www.kickstarter.com/projects/20 ... nicomputer ...

Filter Blog

By date: By tag: