Skip navigation
We will be using quite a lot of image processing on this project, lets make life simple.     It it crazy Just How much miss information there is about opencv and the Raspberry pi, many tutorials will guide you thru a installation process that takes 12 hours+ and has library's linked complexly.   Opencv 2.4.1 [CV2] is available in the default Rasbian Reposttory. To Install on Rasbian, type the following into the command terminal:   Type Into Terminal Sudo apt-get update sudo a ...
Why enter the competition >I have checked out a few of the other Halloween projects and they are great! >Many fun Halloween pi ideas just wont leave the back of my mind >The Element14 Challenges are Fun     Project Scope Right, well I’m guessing you have watched the above video. Lets talk about the plan in a little more detail.   Aim: Pi based vision based project that is scary, fun and would make a great project for people interested in the Rpi and vision. I g ...
With running this project on a non existent budget, a lot of the stuff is going to have be  $1 or borrowed temp from another project.   Here is the poor mans "Fog" build. I built this unit as a pesticide doser, by just adding water it will create safe cool mist and by adding a few delivery hoses we should be able to route this wherever it is needed.   Take a look at the Vertical Growing Blog for more info on this mister:   Automated Green House Blog's Home Page [Updated: 6/ ...
This will be the home page for the automated_Grim Project, a part of the PumpKinPi2015 Competition.       Blogs: Animated_Grim Blog:1 - Project Overview  Animated_Grim Blog:2 - Cheap Fog  Animated_Grim Blog:3 - Raspbery Pi and OpenCv the Easy Way  Animated_Grim Blog:4 - Unboxing The Kit  Animated_Grim Blog:5 - Halloween is upon us  Animated_Grim Blog:6 - Wiring diagram and the skull  Animated_Grim Blog:7 - Pi and Face Detection [Or Anything you want ...

Filter Blog

By date: By tag: