Skip navigation
I'm looking at building an AoIP link using a pair of suitable Rpi's with Wolfson / Cirrus audio boards.   Audio In/Out would be analog. The Ethernet link would be extended using Ubiquity wireless long range access point devices set up as a wireless bridge.   I'm getting a wee bit lost trying to determine the most suitable combination of Rpi board, audio board, and OpenOB version. I also have a strong preference for a board combination that is drop-in compatible with an existing & ...
In the previous parts of this series we've setup a shared network folder and some network nodes. Now we can actually get on with installing and using Blender.   Installation To install blender the following is needed.   sudo apt-get install blender   Running Blender As Blender is a graphical program, it made sense to attach a screen to my controller node and launch the application. It takes a while to launch but eventually it returned the default scene of a cube and a light. Even ...
As shabaz mentioned in the previous comments a lot of the setup for a Pi Cluster applies to other scenarios. Something I stumbled upon this week was building a hadoop cluster with raspberry pi which is another thing you could do with the Bitscope blades.   In this part of the project, I'm looking at the setting up of the nodes.   SSH I took a slightly different approach to enabling SSH on the nodes by creating a file called ssh on each of the boot partition of the SD cards.   Ne ...

Filter Blog

By date: By tag: