Skip navigation
Originally posted on: Pi Zero Case One-Minute Mod – Frederick Vandenbosch   A 1-minute mod for the official Raspberry Pi Zero case, inspired by the ZeroView.   Requires: Raspberry Pi Zero (W) with official case Raspberry Pi Camera module Hobby knife Two suction cups   Follow me: ...
Hello! I'm currently designing a project based off of the Nintendo Switch and modern gaming tablets, It's called PiTab (Pie-Tab) and it uses the Raspberry Pi 3 Model B. It has two slots for controllers on the sides, and a screen in the middle. It also has a 3.5mm headphone jack, an HDMI out, and a rechargeable battery. Why have a rechargeable battery? It's made to be taken with you on the go, not just at home! There's two ways to play; connect it to the dock, or play as a handheld. You can als ...

Filter Blog

By date: By tag: