Skip navigation

Raspberry Pi Projects

3 Posts authored by: aaroNiGHTS
The primary advantage of the Raspberry Pi NoIR camera is seeing in complete darkness. By using an Infrared light source - completely invisible to the human eye - images and videos can be captured with no visible illumination whatsoever.   This video was shot in complete darkness with the new NoIR V2 camera. All illumination comes from two Infrared LEDs powered from the Raspberry Pi itself. It's an example of a common use of night vision - security and surveillance.   A rather shifty ...
No I.R. Despite its name, the new NoIR V2 camera for the Raspberry Pi isn't something designed for filming 1940's mobster movies. What makes it special isn't an additional feature, but rather what it lacks. Most digital cameras are designed to capture images in the same spectrum of light as a normal human eye, producing realistic photos and videos. While cameras can view light outside of this range, filters are use to ensure that only the desired light makes it in the final image. The NoIR ca ...
The Raspberry Pi has been a huge phenomenon in the maker scene, spawning a wide range of accessories, add-ons and even specialised 'Hats'. One of the most underappreciated peripherals would have to be the small Raspberry Pi camera board. At first look it might seem to be the same as any cheap USB camera, but its functionality is far beyond that. The special 15 pin ribbon cable the camera board uses enables it to interface directly with the graphics processor on a Raspberry Pi. This allows it to ...

Filter Blog

By date: By tag: