Skip navigation
(Above) The Advanced Theremin as I had it set up. I placed the sensors separate to allow each hand to control a tone. (via me)     The last BBC Micro:bit Theremin project had you create a single channel for sound. This, “ADVANCED,” Theremin will up that to two channels. The idea here is to create two different tones at the same time. One high pitched and the other lower.     The software works as follows: - When the Micro:bit powers up, you set the ambient lig ...
So, Parallax is collaborating with the National Integrated Cyber Education Research Center to create a cyber:bot using the BBC micro:bit and the Parallax Boe-Bot chassis.  Since this is using the micro:bit, MicroPython is used to program the bot in Python.   This will be a great educational tool to teach both programming and robotics.   On Jan 24, 2019 2:00 PM in Pacific Time (US and Canada) Parallax will hold a Webinar showing a preview of the cyber:bot.   Follow the ...