Skip navigation
__ryanmcclure

PetBud - May Update

Posted by __ryanmcclure May 11, 2018
So far a few problems with regards to setting up the board have been encountered, these are discussed below:   Challenges In order to setup and configure the WaRP 7 board there are an array of procedures involved which can vary in their stages dependant on what software and computer you are using. We first tried to get the board configured using MAC OS Sierra, however, it proved to be troublesome using this host machine setup. This was due to a few issues surrounding the configurability b ...
TLMoto is a team of students from Instituto Superior Técnico, Lisbon, Portugal. Our main goal is to build a fully electric motorcycle to participate the Motostudent International Competition, which happens every two years in the Motorland Aragon MotoGP Circuit.   Our team was created in 2012 and competed in 2014 in the Petrol category (as there was no electric category at the time).  Now, we are building our first electric Motorcycle and will participate this October in the Mot ...
The team has been hard at work during April with the focus on preparing the robot for testing very soon. We made some great progress on the electrical system and the manipulators.   Electrical Updates Having received the PCBs and the electronic components from Farnell, earlier in April, the electrical team started assembling the custom boards.   The first of these boards is the Communication Board, which is responsible for all interfacing between the Microcontroller and the Surface Com ...