Version 3

    New Conductivity Sensor from IST


    June 18, 2010

     

    New Product

     

    IST has employed thin film technology to develop a conductivity sensor for measuring the concentration of ions in an electrolyte. By measuring the voltage drop between two current electrodes, the conductivity of a substance can be determined. The operating temperature range of the sensor is 0°C to +90°C, and its measurement range is ~5μS/cm to ~20mS/cm.


    Temperature Compensation


    The conductivity sensor developed by IST consists of two current electrodes, two measuring electrodes and a platinum temperature sensor for compensation. The sensor has an integrated class B 100Ω or 1000Ω temperature sensor. Since the conductivity of an electrolyte depends heavily on the temperature of the medium, it is important to have accurate temperature compensation. The platinum RTD is located on the sensor, directly at the point of measurement to assure accuracy.

    Applications in Water Quality


    Conductivity sensors have an important application in determining water quality, measuring the concentration of ions found in the water. IST's conductivity sensor is ideal for this application as well as other applications to measure the conductivity of an electrolyte. The sensors are able to measure the conductivity of most electrolytes, excluding those that are volatile to platinum.

     

    Conductivity Sensor Data Sheet (PDF 93,0 kB)