Version 20
    MCU/MPU/DSP > Development Platforms & Kits > Daughter / Add-on boards >
    • USB-TO-GPIO USB Interface Adapter Evaluation Module
    • USB-TO-GPIO USB Interface Adapter Evaluation Module
    • USB-TO-GPIO USB Interface Adapter Evaluation Module

    Overview

    The USB-TO-GPIO Evaluation Module serves as an interface adapter or a bridge between a host PC (IBM™ compatible) and one or multiple slave devices via a standard type-A to mini-B USB cable. The communication between the USB interface adapter and the host PC is via USB, while the communication between the USB interface adapter and the slave device(s) is via an inter-integrated circuit (I²C), SMBus, PMBus and/or general-purpose inputs/outputs GPIOs. The bridge converts communication transactions between the USB and serial protocol.

    The adapter solution includes a set of PC libraries and a GUI that can be used to allow PC applications access to the adapter and target devices that the adapter supports. The GUI and PC libraries are designed using the Microsoft® .NET Framework, in order to leverage as many standard libraries as possible. The adapter presents itself as a USB HID to Windows, Because of this, no custom driver is required, and the application software on the PC can use the standard Microsoft Windows USB driver (usbhid.sys).

    Like the adapter, the Windows libraries support all the different types of device interfaces: I2C, SMBus, PMBus, and GPIO. In addition, the libraries support configuration and control of the adapter itself by allowing PC programs to update the EERPROM in the adapter, select switching in and out of resistors on data and clock lines, etc.

    Key Applications: Graphic User Interface

    Features

    • Supports master mode I²C, SMBus or PMBus as well as GPIO.
    • Supports USB1.1 full speed at 12 Mbit/s. The USB interface adapter is recognized by the host as a generic human interface device (HID), so no proprietary USB or HID driver is needed. Therefore, the USB interface adapter can be treated as a USB plug-and-play device.
    • Selects different clock speeds (either 100 kHz or 400 kHz) for I²C, PMBus, or SMBus communications.
    • Configures different pullup resistors for clock, data and ALERT signals (including open-drain).
    • Supports flexible I²C read or write transactions (specify raw data, instead of device address, command, etc.) .
    • Includes .NET DLL for supporting Windows .NET GUIs using the adapter.
    • No Windows dependencies other than the Microsoft .NET Framework version 2.0.

    Ships With

    • USB-TO-GPIO Module
    • Cables