Version 2

    element14


    Freedom Beginners Guide


    The purpose of the “Freedom” Board Platform is to provide a low-cost ($10-15 MSRP) evaluation and development platform for Freescale MCUs and the Tower System should be considered as a development platform offering extended options (external components, connectors, accessories).

    The Freedom boards will be simple but useful with quick but effective out-of-box demo options. The goals of the design are to provide:

    • easy access to MCU I/O
    • battery-ready, low-power operation
    • power-measurement access points
    • standard-based form factor with expansion board options
    • built-in debug interface for flash programming and run-control


    Contents

     

    1. Introduction to ARM MCU Cores
    1.1 ARM Processor Architecture overview
    1.2 ARM Cortex Microcontroller Families
    1.3 ARM Cortex-M0+ core module details
    1.4 ARM Cortex-M4 core module details
    2. Kinetis MCUs based on ARM Technology
    2.1 Kinetis series overview
    2.2 Kinetis K-Series MCUs
    2.2.1. Kinetis K Series Portfolio Details
    2.2.2 Freescale Development Tool Part Numbers for K series
    2.3 Kinetis L-Series MCUs
    2.3.1 Kinetis L series portfolio details
    2.3.2 Freescale Development Tool Part Numbers for L series
    2.4 Kinetis E-series MCUs
    2.4.1 Kinetis E series Portfolio Details
    2.4.2 Freescale Development Board Part Numbers for E series
    2.5 Kinetis V-Series MCUs for Motor control
    2.6 Kinetis W-Series for Wireless Connectivity
    2.7 Kinetis M-Series for Smart Metering
    3. Freescale Freedom Development Platform
    3.1 List of available Freedom Development boards
    3.2 List of available Freedom Accessory boards
    3.3 Freescale Freedom Board Features Matrix
    3.3.1 FRDM-KL Series Board
    3.3.2 FRDM-KE Series Board
    3.3.3 FRDM-K Series Board
    4 Introduction to the OpenSDA interface
    4.1 OpenSDA MSD Bootloader
    4.2 OpenSDA Application Overview
    4.2.1 OpenSDA as Mass Storage Application
    4.2.2 OpenSDA P&E Debug Application
    4.2.3 OpenSDA Data Logging Application
    4.2.4 OpenSDA + CMSIS-DAP
    4.3 MSD Flash Programmer
    4.3.1 Enter OpenSDA Bootloader Mode
    4.3.2 Load an OpenSDA Application
    4.3.3 Load executables (Flash Programmer)
    5 Complementary Development Board: Freescale Tower System
    6 Freescale’s Microcontroller Enablement
    6.1 Software Development Tools
    6.1.1 Processor Expert Software
    6.1.2 Freescale CodeWarrior Development Studio
    6.1.3  IAR Embedded Workbench
    6.1.4 Keil IDE Microcontroller Development Kit for ARM (MDK-ARM)
    6.2 mbed Development Tools
    6.2.1 mbed SDK
    6.2.2 mbed HDK
    6.2.3 Benefits of the mbed
    6.3 Hardware Development Tools
    6.3.1 Segger Tools
    6.3.2 P&E Micro Tools
    6.3.3 KEIL Tools
    6.4 Operating Systems
    7 Basic Exercise on Freedom Board
    7.1 Freescale Processor Expert - Make FRDM-KL25Z RGB Blink exercise
    7.2 Exercise on mbed - Blinky, Touch Sensor and Accelerometer exercises

     

     

     

    1. Introduction to ARM MCU Cores

     

    ARM is a family of instruction set architectures for computer processors based on a reduced instruction set computing (RISC) architecture developed by British company ARM Holdings. ARM Holdings develops the instruction set and architecture for ARM-based products, but does not manufacture products. The company periodically releases updates to its cores.

    The company is best known for its processors, although it also designs, licenses and sells software development tools under the RealView and KEIL brands, systems and platforms, system-on-a-chip infrastructure and software.

    There are many variants of ARM processors, with different capabilities, and implementing different features. But all of them implement a version of the 'ARM architecture' (ARM ISA), that describes the interface and properties (instruction set, behaviour, etc.) that ARM processors must support. It has been refined over time with successive architecture versions.


    1.1 ARM Processor Architecture overview

     

    ARM architecture forms the basis for every ARM processor. Over time, the ARM architecture has evolved to include architectural features to meet the growing demand for new functionality, high performance and the needs of new and emerging markets.

     

    The ARM architecture supports implementations across a wide range of performance points, establishing it as the leading architecture in many market segments. The ARM architecture supports a very broad range of performance points leading to very small implementations of ARM processors, and very efficient implementations of advanced designs using state of the art micro-architecture techniques. Implementation size, performance, and low power consumption are key attributes of the ARM architecture.

     

    1.jpg

     

    ARM developed architecture extensions to provide support for Java acceleration (Jazelle®), security (TrustZone®), SIMD, and Advanced SIMD (NEON™) technologies. The ARMv8-architecture adds a Cryptographic extension as an optional feature.


    The ARM architecture is similar to Reduced Instruction Set Computer (RISC) architecture, as it incorporates these typical RISC architecture features:

    • A uniform register file load/store architecture, where data processing operates only on register contents, not directly on memory contents.
    • Simple addressing modes, with all load/store addresses determined from register contents and instruction fields only.

    Enhancements to a basic RISC architecture enable ARM processors to achieve a good balance of high performance, small code size, low power consumption and small silicon area.

     

    1.2 ARM Cortex Microcontroller Families

     

    The 32-bit ARM architecture, such as ARMv7, is the most widely used architecture in mobile devices. The architecture has evolved over time, and version seven of the architecture, ARMv7, that defines the architecture for the first of the Cortex series of cores, defines three architecture "profiles". Although the architecture profiles were first defined for ARMv7, ARM subsequently defined the ARMv6-M architecture (used by the Cortex M0/M0+/M1) as a subset of the ARMv7-M profile with fewer instructions.

     

    The latest Cortex family (v7) includes a wider range of processors than earlier families. These processors are suitable for very different kinds of application, and three profiles were therefore introduced to distinguish what targets they are adapted to:

     

    • A-profile applications processors are for full OS. This features powerful processors found in high-end products like Smartphone’s, tablets, or notebooks. This includes the famous Cortex-A8 and Cortex-A9 (in your super phone) processors.

     

    • 'R-profile is Real-time profile processors which can be found for example in control units for automotive systems or hard disk drive controllers. They come with specific features suited to real-time environment constraints. R profile processors have for example a tightly coupled memory, local to the processor that allows for fast-responding code and data. They also all have hardware support for integer division that would otherwise require software emulation.

     

    • The 'M' Micro-controller profile processors are smaller and used in numerous embedded systems like human interface devices, automotive control systems, power management systems, and others.

     

    The ARM Cortex-M is a group of 32-bit RISC ARM processor cores licensed by ARM Holdings. The cores are intended for microcontroller use, and consist of the Cortex-M0, Cortex-M0+, Cortex-M1, Cortex-M3, and Cortex-M4.

    The Cortex-M family is optimized for cost and power sensitive MCU and mixed-signal devices for end applications such as smart metering, human interface devices, automotive and industrial control systems, white goods, consumer products and medical instrumentation.

    1.jpg

    Some of the most important options for the Cortex-M cores are:

    • SysTick Timer: A 24-bit system timer that extends the functionality of both the processor and the Nested Vectored Interrupt Controller (NVIC). When present, it also provides an additional configurable priority SysTick interrupt. Though the SysTick timer is optional, it's rare to see a Cortex-M microcontroller without it.


    • Bit Banding: Maps a complete word of memory onto a single bit in the bit-band region. For example, writing to an alias word will set or clear the corresponding bit in the bitband region. This allows every individual bit in the bit-banding region to be directly accessible from a word-aligned address, and individual bits to be toggled from C/C++ without performing a read-modify-write sequence of instructions.


    • Memory Protection Unit (MPU): Provides support for protecting regions of memory through enforcing privilege and access rules. It supports up to eight different regions, each of which can be split into a further eight equal-size sub-regions.

    1.jpg


    ARM Cortex-M Instruction Sets


    All four Cortex-M cores implement a common instruction subset that consists of: Thumb subset, Thumb-2 subset, and multiply. The Cortex-M0 / M0+ / M1 include all older Thumb instructions, except new instructions (CBZ, CBNZ, IT) which were added in ARMv7-M architecture. The Cortex-M0 / M0+ / M1 include a minor subset of Thumb-2 instructions (BL, DMB, DSB, ISB, MRS, MSR)


    ARM
    Cortex-M

    Thumb

    Thumb-2

    Hardware
    multiply

    Hardware
    divide

    Saturated
    math

    DSP
    extension

    Floating point

    ARM
    architecture

    Core
    architecture

    Cortex-M0

    Most

    Subset

    1 or 32 cycle

    No

    No

    No

    No

    ARMv6-M

    Von Neumann

    Cortex-M0+

    Most

    Subset

    1 or 32 cycle

    No

    No

    No

    No

    ARMv6-M

    Von Neumann

    Cortex-M1

    Most

    Subset

    3 or 33 cycle

    No

    No

    No

    No

    ARMv6-M

    Von Neumann

    Cortex-M3

    Entire

    Entire

    1 cycle

    Yes

    Yes

    No

    No

    ARMv7-M

    Harvard

    Cortex-M4

    Entire

    Entire

    1 cycle

    Yes

    Yes

    Yes

    Optional

    ARMv7E-M

    Harvard

                                                             1.jpg

    1.3 ARM Cortex-M0+ core module details

     

    The ARM® Cortex®-M0+ processor is the most energy efficient ARM processor available. It builds on the very successful Cortex-M0 processor, retaining full instruction set and tool compatibility, while further reducing energy consumption and increasing performance. Along with the Cortex-M0 processor, the exceptionally small silicon area, low power and minimal code footprint of these processors enable developers to achieve 32-bit performance at an 8-bit price point, bypassing the step to 16-bit devices. The Cortex-M0+ processor comes with a wide selection of options to provide flexible development.

    1.jpg

     

    Below are the features of Cortex-M0+ core:

     

    • Supports up to 32 interrupt request sources
    • 2-stage pipeline micro architecture for reduced power consumption and improved architectural performance (cycles per instruction)
    • Binary compatible instruction set architecture with the Cortex-M0 core
    • Thumb instruction set combines high code density with 32-bit performance
    • Serial wire debug (SWD) reduces the number of pins required for debugging
    • Single cycle 32 bits by 32 bits multiply

    Nested Vectored Interrupt Controller (NVIC)

    • Up to 32 interrupt sources
    • Includes a single non-maskable interrupt

    Asynchronous Wake-up Interrupt Controller (AWIC)

    • Supports interrupt handling when system clocking is disabled in low-power modes
    • Takes over and emulates the NVIC behavior when correctly primed by the NVIC on entry to very deep sleep mode.
    • A rudimentary interrupt masking system with no prioritization logic signals for wake-up as soon as a non-masked interrupt is detected
    • Contains no programmer’s model visible state and is therefore invisible to end users of the device other than through the benefits of reduced power consumption while sleeping


    The Cortex-M0+ is an optimized superset of the Cortex-M0. The Cortex-M0+ has complete instruction set compatibility with the Cortex-M0 thus allowing one to use the same compiler and debug tools. The Cortex-M0+ pipeline was reduced from 3 to 2 stages, which lowers the power usage. In addition to debug features in the existing Cortex-M0, a silicon option can be added to the Cortex-M0+ called the Micro Trace Buffer (MTB) which provides a simple instruction trace buffer. The Cortex-M0+ also received Cortex-M3 and Cortex-M4 features, which can be added as silicon options, such as the memory protection unit (MPU) and the vector table relocation. Key features of the Cortex-M0+ core are:

    • ARMv6-M architecture
    • Instruction sets (same as Cortex-M0)
      • Thumb (most), missing CBZ, CBNZ, IT.
      • Thumb-2 (subset), only BL, DMB, DSB, ISB, MRS, MSR.
      • 32-bit hardware multiply, 1-cycle or 32-cycles (silicon option)
      • 2-stage pipeline (one less than Cortex-M0)
      • 11.21 µW/MHz dynamic power requirement
      • Silicon options:
        • Micro Trace Buffer (MTB) (unique to Cortex-M0+)
        • Single-cycle I/O port (unique to Cortex-M0+)
        • Vector table relocation (same as Cortex-M3 and Cortex-M4)
        • 8 region memory protection unit (MPU) (same as Cortex-M3 and Cortex-M4)

     

    ISA SupportThumb® / Thumb-2 subset
    Pipeline2 stage
    Performance Efficiency

    2.42 CoreMarks/MHz*

    Performance Efficiency

    0.95 / 1.11 / 1.36 DMIPS/MHz**

    Memory Protection

    Optional 8 region MPU with sub regions and background region

    Interrupts

    Non-maskable Interrupt (NMI) + 1 to 32 physical interrupts

    Sleep Modes

    Integrated WFI and WFE Instructions and Sleep On Exit capability
    Sleep & Deep Sleep Signals
    Optional Retention Mode with ARM Power Management Kit

    Bit Manipulation

    Bit banding region can be implemented with Cortex-M System Design Kit

    Enhanced Instructions

    Hardware single-cycle (32x32) multiply option

    Debug

    Optional JTAG or Serial-Wire Debug Ports Up to 4 Breakpoints and 2 Watchpoints

    Trace

    Optional Micro Trace Buffer

     

    1.4 ARM Cortex-M4 core module details

     

    The ARM® Cortex®-M4 processor is the latest embedded processor by ARM specifically developed to address digital signal control markets that demand an efficient, easy-to-use blend of control and signal processing capabilities.

    The combination of high-efficiency signal processing functionality with the low-power, low cost and ease-of-use benefits of the Cortex-M family of processors is designed to satisfy the emerging category of flexible solutions specifically targeting the motor control, automotive, power management, embedded audio and industrial automation markets.

    1.jpg

     

    The Cortex-M4 processor has been designed with a large variety of highly efficient signal processing features applicable to digital signal control markets.  The Cortex-M4 processor features extended single-cycle multiply accumulate (MAC) instructions, optimized SIMD arithmetic, saturating arithmetic instructions and an optional single precision Floating Point Unit (FPU).

    The processor executes the Thumb®-2 instruction set for optimal performance and code size, including hardware division, single cycle multiply, and bit-field manipulation. The Cortex-M4 Nested Vectored Interrupt Controller is highly configurable at design time to deliver up to 240 system interrupts with individual priorities, dynamic reprioritization and integrated system clock.


    Conceptually the Cortex-M4 is a Cortex-M3 plus DSP Instructions, and optional floating-point unit (FPU). If a core contains an FPU, it is known as a Cortex-M4F, otherwise it is a Cortex-M4. Key features of the Cortex-M4 core are:


    • ARMv7E-M architecture
    • Instruction sets
      • Thumb (entire)
      • Thumb-2 (entire)
      • 1-cycle 32-bit hardware multiply, 2-12 cycle 32-bit hardware divide, saturated math support
      • DSP extension: Single cycle 16/32-bit MAC, single cycle dual 16-bit MAC, 8/16-bit SIMD arithmetic.
      • Floating-point extension (silicon option): Single-precision floating point unit, IEEE-754 compliant. This is called the FPv4-SP extension.
    • 3-stage pipeline with branch speculation
    • 1 to 240 physical interrupts, plus NMI
    • 12 cycle interrupt latency
    • Integrated sleep modes
    • 8 region memory protection unit (MPU) (silicon option)
    • 1.25 DMIPS/MHz

     

    ISA SupportThumb® / Thumb-2
    DSP ExtensionsSingle cycle 16,32-bit MAC
    Single cycle dual 16-bit MAC
    8,16-bit SIMD arithmetic
    Hardware Divide (2-12 Cycles)
    Floating Point UnitSingle precision floating point unit
    IEEE 754 compliant
    Pipeline3-stage + branch speculation
    Performance Efficiency

    3.40 CoreMark/MHz*

    Performance Efficiency

    Without FPU: 1.25 / 1.52 / 1.91 DMIPS/MHz**
    With FPU: 1.27 / 1.55 / 1.95 DMIPS/MHz**

    Memory Protection

    Optional 8 region MPU with sub regions and background region

    Interrupts

    Non-maskable Interrupt (NMI) + 1 to 240 physical interrupts

    Interrupt Priority Levels

    8 to 256 priority levels

    Wake-up Interrupt Controller

    Up to 240 Wake-up Interrupts

    Sleep Modes

    Integrated WFI and WFE Instructions and Sleep On Exit capability.
    Sleep & Deep Sleep Signals.
    Optional Retention Mode with ARM Power Management Kit

    Bit Manipulation

    Integrated Instructions & Bit Banding

    Debug

    Optional JTAG & Serial-Wire Debug Ports. Up to 8 Breakpoints and 4 Watchpoints.

    Trace

    Optional Instruction Trace (ETM), Data Trace (DWT), and Instrumentation Trace (ITM)

     

     

    2. Kinetis MCUs based on ARM Technology

     

    Freescale is the leader in 32-bit embedded control, offering the market’s broadest and best-enabled portfolio of solutions based on ARM® technology. ARM-powered portfolio includes scalable MCU and MPU families from small ultra-low power Kinetis MCUs to i.MX and Vybrid applications processors with advanced performance and feature integration and QorIQ communications processors that deliver industry-leading power and performance. Each family has been designed to offer a broad range of performance, peripheral and packaging options, providing migration paths for end-product platform development.

    Freescale's Kinetis portfolio of ARM® Cortex™ MCUs consists of multiple hardware- and software-compatible ARM® Cortex™-M0+ and ARM® Cortex™-M4 MCU families with exceptional low-power performance, memory scalability and feature integration. Families range from the entry-level ARM® Cortex™-M0+ Kinetis L Series to the high-performance, feature-rich ARM® Cortex™-M4 Kinetis K and include a wide selection of analog, communication, HMI, connectivity and security features.


    All Kinetis MCUs are supported by a comprehensive Freescale and third-party hardware and software enablement system which reduces development costs and time to market.

     

    2.1 Kinetis Series Overview

     

    Below shows different Kinetis series family of devices with core and application specific details.

             1.jpg

     

    2.2  Kinetis K-Series MCUs

     

    Freescale's Kinetis K series MCU portfolio includes more than 600 compatible low-power, high-performance 32-bit MCUs built on the ARM® Cortex®-M4 core. This series is designed for scalable performance, integration, connectivity, communications, HMI and security and offers additional features for exceptional integration with multiple fast 16-bit analog-to-digital converters (ADCs), digital-to-analog converters (DACs) and a programmable-gain amplifier (PGA), along with powerful, cost-effective signal conversion, conditioning and control. These MCU families are performance efficient, offer industry-leading low power, and provide significant BOM savings through the smart on-chip integration.


    Scalability – Over 200 hardware and software compatible ARM Cortex-M4 MCUs with DSP + low-power, connectivity, communications, HMI and security features

    Mixed Signal – Exceptional integration with fast 16-bit ADCs, DACs, PGAs and more. Powerful, cost-effective signal conversion, conditioning and control 

    Flex Memory – Fast, low-power 90nm Thin-Film Storage Flash. Innovative FlexMemory technology delivers fast, flexible, high-endurance on-chip EEPROM

    Enablement – Freescale bundled MQX RTOS and CodeWarrior IDE with Processor Expert auto code generator. 3rd party support from IAR, KEIL and other ARM ecosystem providers.


    Common Features of KL series MCU are:

    System

    • ARM® Cortex™-M4 core with FPU, MAC, SIMD
    • Multiple low power modes and peripherals, low-power boot, clock gating
    • Powerful DMA and X-bar switch enabling parallel Processing
    • 200 μA/MHZ in run modes, fast wake up times, 690 to 2μA in lower power Stop and 10 modes of operation to balance performance and power
    • 1.71 to 3.6 V voltage supply with full access to analog and memory across full range
    • –40° C to +105° C

    Memory

    • Up to 1 MB of flash memory
    • Single cycle access to flash
    • Optional EEPROM
    • MPU and flash swap controller to enable robust firmware updates
    • CRC module
    • DRAM and NAND flash I/F

    Rich Mixed Signal

    • Up to 4 x configurable 16-bit ADCs supporting on-chip PGAs
    • High-speed analog comparator with integrated 6-bit DAC
    • 12-bit DAC
    • FlexTimers for ICAP, OCOMP and PWM

    Connectivity

    • 10/100 BaseT Ethernet MAC with stacks supporting IPV6
    • USB2.0 OTG module
    • Up to 2 x FlexCAN, 2.0B compliant
    • Up to 6 UART, support available for smart card plus Manchester Encoding
    • Up to 3 SPI with chip selects
    • I2S or Serial Audio I/F
    • I2C
    • SDIO I/F

    Security

      • Hardware encryption accelerator
      • Random number generator
      • Anti-tamper circuitry to monitor and help prevent application tampering and to protect your IP

    HMI

      • Graphics controller supporting SVGA resolution
      • Parallel bus for camera I/F
      • Capacitive touch sense module

     

    2.2.1. Kinetis K Series Portfolio Details

    1.jpg

    Kinetis K Series MCUs Family Compatibility: Hardware & software compatible MCU families with scalable performance, memory and feature integration

    1.jpg

    2.2.2 Freescale Development Tool Part Numbers for K series


    Freescale Tower Development Board Part Numbers


    Tower Module Part Number

    Kinetis Family Support

    Buy Here

    Extended H/W Support Options

    TWR-K20D50M

    50 MHz MK10 and MK20

    Buy

     

     

     

     

    802.11.x, Serial Connectivity, Analog, Sensors, Graphics LCD, Audio, Tower Dock (iPad®, iPhone®, iPod®), General I/O, 2.4GHz and Sub 1 GHz RF, Modules, Motor Control, Memory Modules etc.

    TWR-K21D50M

      50 MHz MK11, MK12, MK21 and MK22

    Buy

    TWR-K20D72M

    72 MHz MK10 and MK20

    Buy

    TWR-K21F120M

    120 MHz MK21 and MK22

    Buy

    TWR-K40D100M

    100 MHz MK30 and MK40

    Buy

    TWR-K40X256

    100 MHz MK30 and MK40

    Buy

    TWR-K53N512

    All MK50, MK51, MK52 & MK53 variants

    Buy

    TWR-K60D100M

    100 MHz MK10, MK20 and MK60

    Buy

    TWR-K60F120M

    120/150 MHz MK10, MK20

    and MK60

    Buy

    TWR-K60N512

    K10, K20 and K60, 100MHz

    Buy

    TWR-K60N512-IAR

    IAR Kick Start Kit for Kinetis K60 family

    Buy

    TWR-K60N512-KEIL

        Keil Starter Kit for Kinetis K60 family

    Buy

    TWR-K64F120M

    K64, 120MHz

    Buy

    TWR-K70F120M

    120/150 MHz MK61 and MK70

    Buy

     

    Freescale Freedom Development Board Part Numbers

     

    Freedom board Part Number

    Kinetis Family Support

    Buy Here

    Extended H/W Support Options

    FRDM-K64F

       Kinetis K MCU, K64, 120 MHz

    Buy

     

    Arduino shields

    footprint

    FRDM-K20D50M

    Kinetis K MCU, K20, 50MHz

    Buy

    FRDM-K22F

       Kinetis K MCU, K22, 120 MHz

    Buy

     

     

    2.3  Kinetis L-Series MCUs

     

    Kinetis L series MCUs are the world’s most energy efficient, bringing new design possibilities to entry-level applications that have previously been limited by 8/16-bit MCU capabilities. Kinetis L series MCUs combine the enhanced energy efficiency, performance and debug features of the new 32-bit ARM Cortex-M0+ core, with the scalability, feature integration and enablement of the Kinetis MCU portfolio. Available with multiple flash memory options and a rich selection of analog, connectivity and HMI peripherals, Kinetis L series MCUs are also hardware and software compatible with Kinetis K series MCUs based on the ARM Cortex™-M4 core. Both are supported by an industry-leading Freescale enablement package that includes the CodeWarrior IDE with Processor Expert tool, Freescale Freedom development platform and MQX™ Lite RTOS, as well as the ARM third-party ecosystem.

    Ultra-low Power

    Architected for power efficiency, the Kinetis L series takes advantage of ARM’s ultra-low-power Cortex-M0+ processor and features peripherals that help you optimize power consumption.

     

    Super Simple
    Its 32-bit functionality with 8-bit ease-of-use. Built on the new ARM Cortex-M0+ core (the smallest, lowest-power ARM core), the L series simplifies development with an upward migration path to Kinetis K and X series, software reuse and flexible power optimization. And, with a comprehensive enablement bundle including CodeWarrior IDE, MQX RTOS and the ARM support ecosystem, development is simple.


    Leading Scalability and Integration

    Expanding on well-known features of the Kinetis platform with leading scalability, best-in-class integration with rich analog features and low-power connectivity, the L series redefines entry-level.

     

    Common Features of KL series MCU are :

    System

    • ARM® Cortex™-M0+ core, 48 MHz
    • Multiple low power modes and
    • peripherals, low-power boot,
    • clock gating
    • 1.71–3.6 V, –40° C to +105° C

    Memory

    • 90 nm TFS flash, SRAM
    • Internal memory security/protection

    Analog Peripherals

    • 12/16-bit ADC, 12-bit DAC
    • High-speed comparator

    Serial Interfaces

    • UART (including 1 LPUART)
    • SPI, I2C

    Timers

    • Real-time clock
    • 16-bit low-power TPMs (GP timer/PWM)
    • Low-power timers
    • 32-bit periodic interrupt timer

     

    2.3.1  Kinetis L series portfolio details


    1.jpg

     

    Choosing the Right Kinetis ARM Cortex-M MCU’s (K and L series)

    1.jpg

    2.3.2 Freescale Development Tool Part Numbers for L series


    Freescale Freedom Development Board

     

    • Ultra-low-cost development platforms

    • Quick and simple with easy access to MCU I/O and including a capacitive touch slider and accelerometer

    • Form factor compatible with popular third-party hardware designed to work with Arduino™ and Arduino-compatible boards

    • New, sophisticated OpenSDA Debug interface: Mass storage device flash programming interface, P&E Multilink interface for run-control debugging,

    open-source data logging application

    • Loaded with software, including Processor Expert: Stand-alone or IDE integrated, MQX Lite RTOS (via Processor Expert) and ecosystem partner support from IAR, Keil, Code Red, Atollic, Rowley, Free GNU command line tools with GDB server


    Part Number

    Supporting Families

    Buy Here

    FRDM-KL02Z

    KL02

    Buy

    FRDM-KL05Z

    KL04/05

    Buy

    FRDM-KL25Z

    KL14/15/24/25

    Buy

    FRDM-KL26Z

    KL16/26 up to 128 KB flash

    Buy

    FRDM-KL46Z

    KL16/26 at 256 KB flash and KL34/36/46

    Buy

     

     

    Freescale Tower System Platforms for Kinetis L series MCUs

     

    • Modular, open-source development platform with reusable peripheral modules offering connectivity, analog, graphics LCD and motor control functionality

    • Tower plug-in (TWRPI) socket

    • OpenSDA debug circuit with virtual serial port

    • MMA8451Q accelerometer

    • Tower elevator modules (TWR-ELEV) and Tower peripheral modules (TWR-SER, TWR-PROTO, etc.) pictured, are ordered separately for additional system capability

     

    Part Number

    Supports Families

    Buy Here

    TWR-KL25Z48M

    KL14/15/24/25

    Buy

    TWR-KL46Z48M

    KL16/26 at 256 KB flash and KL34/36/46

    Buy

     

    2.4 Kinetis E-series MCUs

     

    The Kinetis E series is the most scalable portfolio of ARM® Cortex®-M0+ MCUs in the industry. Designed to maintain high robustness for complex electrical noise environments and high-reliability applications, the Kinetis E series families offer a broad range of memory, peripheral and package options. They share common peripherals and pin counts allowing developers to migrate easily within an MCU family or between MCU families to take advantage of more memory or feature integration. This scalability allows developers to standardize on the Kinetis E series for their end product platforms, maximizing hardware and software reuse and reducing time-to-market.


    Strong Robustness EMC/ESD design technology ensure strong noise immunity performance

    High Efficiency Cortex-M0+ core up to 48MHz and 40x more than 8/16-bit MCUs

    Low Cost Optimized for cost-sensitive applications offering low pin count option

     

    General Features of Kinetis E series MCU:

    • 32-bit ARM Cortex-M0+ core
    • Scalable memory footprints from 8 KB flash / 1 KB SRAM to 128 KB flash / 16 KB SRAM
    • Precision mixed-signal capability with on chip analog comparator and 12-bit ADC
    • Powerful timers for a broad range of applications including motor control
    • Serial communication interfaces such as UART, SPI, I²C, etc.
    • High security and safety with internal watchdog and programmable CRC module
    • Single power supply (2.7–5.5 V) with full functional flash program/erase/read operations
    • Ambient operation temperature range: -40 °C ~ 105 °C
    • Robust 5 V MCU (high electrical noise environments) with 8-bit S08 compatibility
    • System safety peripherals for high reliability applications

     

    Common Features of the core


    Operating characteristics

    • 2.7 V to 5.5 V
    • Temperature range (TA) -40 °C to 105 °C
    • Three operation modes: Run, Wait, Stop

    Core features

    • Next generation 32-bit ARM Cortex M0+ core
    • Support up to 32 interrupt request sources
    • Nested vectored interrupt controller (NVIC)
    • 2-pin serial wire debug (SWD) interface

    System and power management

    • Watchdog
    • Integrated bit manipulation engine (BME)
    • Power management controller with three different
    power modes
    • Non-maskable interrupt (NMI)
    • 64-bit unique identification (ID) number per chip

    Clocks

    • External crystal oscillator or resonator
    • DC- 20 MHz external square wave input clock
    • Internal clock references
    • 31.25–39.063 kHz oscillator
    • 1 kHz oscillator
    • Frequency-locked loop with the range of
    • 16–20 MHz

    Memory and memory interfaces

    • Up to 64 KB flash memory
    • Up to 256 B EEPROM
    • Up to 4 KB random-access memory

    Security and integrity

    • Watchdog (WDOG)
    • One cyclic redundancy check (CRC) module

     

     

    2.4.1 Kinetis E-Series Portfolio Details

    1.jpg

     

    2.4.2 Freescale Development Board Part Numbers for E-Series


    Part Number

    Kinetis Family

    Buy Here

    FRDM-KE02Z

    KE02, 20 MHz

    Buy

    FRDM-KE02Z40M

    KE02, 40 MHz

    Buy

    FRDM-KE04Z

    KE04, 8 KB Flash

    Buy

    FRDM-KE06Z

    KE06, KE04, 64-128 KB Flash

    Buy


    2.5 Kinetis V-Series MCUs for Motor control

     

    Kinetis V Series MCUs are based upon the ARM® Cortex®-M0+ and M4 cores and are designed for BLDC, PMSM and ACIM motor control, as well as digital power conversion applications. The Kinetis KV1x family is the entry point and features a 75 MHz ARM Cortex-M0+ core with a hardware square root and divide block giving it a 27% increase in performance vs. comparable 32-bit MCUs in sensorless PMSM control.


    With an ARM Cortex-M4 core, floating point unit and clock frequencies of up to 150 MHz, the Kinetis KV3x and Kinetis KV4x families extend the V series to higher dynamic control systems including those with multiple motors. Kinetis V Series features include dual 16-bit analog-to-digital converters (ADCs) sampling at up to 1.2 mega samples per second (MS/s) in 12-bit mode, multiple motor control timers and 16-512 KB of flash memory. The Kinetis KV4x family includes advanced analog and timing peripherals from Freescale's digital signal controller (DSC) portfolio to address the requirements of digital power conversion applications. All families are supported by a full enablement suite from Freescale and third-party resources, including reference designs, software libraries and motor configuration tools.


    Freescale Development Board Part Numbers for V-Series


    Part Number

    Kinetis Family

    Buy Here

    TWR-KV10Z32

    KV1x, 75 MHz

    Buy

    TWR-KV31F120M

    KV3x, 120 MHz

    Buy


    2.6 Kinetis W-Series for Wireless Connectivity

     

    The Kinetis W series integrates class-leading sub-1 GHz and 2.4 GHz RF transceivers with ARM® Cortex® cores, providing robust feature sets for reliable, secure and low-power embedded wireless solutions. The Kinetis W series is optimized for wireless, providing the right mix of performance, integration, connectivity and security. The enablement packages include Freescale's Tower System Development Platforms, MQX™ RTOS and support from IAR Systems. Whether you need sub-1 GHz or 2.4 GHz wireless, simple point-to-point or full mesh networking, the Kinetis W series has the solution to fit your needs.


    • ARM Cortex-M + Wireless Transceiver
    • Sub-1 GHz and 2.4 GHz wireless platforms
    • Compatible with “K” series peripherals
    • Leverage “K” series tools for design and debug

     

    Freescale Development Tool Part Numbers for W-Series


    Part Number

    Kinetis Family

    Buy Here

    TWR-KW21D256

    KW2x MCUs

    Buy

    TWR-KW24D512

    Kinetis KW2x

    Buy


    2.7 Kinetis M-Series for Smart Metering

     

    Kinetis M series MCUs are based upon the low-power ARM® Cortex®-M0+ core and are designed for single-chip 1, 2 and 3 -phase electricity meters as well as flow meter and other precision measurement applications.

    Kinetis M Series MCUs include a powerful analog front end consisting of multiple 24-bit Sigma Delta ADCs, Programmable Gain Amplifiers, voltage reference with low drift over temperature and a phase shift compensator. A large range of security features including a memory protection unit, external tamper detection pins, iRTC with tamper detect and a random number generator provide protection of supplier/user data within the MCU and from the MCU to the power grid. A low power segment LCD controller support up to 288 segments and 8 backplanes.


    • ARM Cortex-M0+ Core
    • Multiple high-precision 24-bit ΣΔ ADCs with PGAs
    • Hardware Current Transformer phase shift compensation
    • Robust Tamper Detection Circuitry & Low Power Segment LCD
    • 50MHz, up to 128KB, 100pin

     

    Freescale Development Tool Part Numbers for M-Series


    Part Number

    Kinetis Family

    Buy Here

    TWR-KM34Z50M

    KM3x and KM1x, 50MHz

    Buy


    3. Freescale Freedom Development Platform

     

    The Freescale Freedom development platform is a small, low-power, cost-effective evaluation and development system perfect for quick application prototyping and demonstration ofKinetis MCU families. The platform offers an easy-to-use mass-storage device mode flash programmer, a virtual serial port and classic programming and run-control capabilities.

    • Low–cost (<$20 USD MSRP)
    • Designed in an industry-standard compact form factor
    • Easy access to the MCU I/O pins
    • Integrated open-standard serial and debug interface (OpenSDA)
    • Compatible with a rich-set of third-party expansion boards

    It's easy to get started. Simply choose your preferred Freescale Freedom development hardware, select compatible software, connect with the community, and go.

     

    3.1 List of available Freedom Development boards

     

     

     

     

    3.2 List of available Freedom Accessory boards

     

    The Freedom development platform is form factor compatible with the Arduino R3 shields.

    Some shield drivers have already been ported for certain FRDM boards and will be easily modifiable between each FRDM board. In the other side, it should not be a huge effort to migrate the existing shield drivers (available for the ATMega Arduino MCU boards) to the FRDM boards.
    Below are the shields with a FRDM driver available:

     

    3.3 Freescale Freedom Board Features Matrix

     

     

    3.3.1 FRDM-KL Series Board

     

     

    FRDM-KL02Z

    FRDM-KL05Z

    FRDM-KL25Z

    FRDM-KL26Z

    FRDM-KL46Z

    MCU Part No

    MKL02Z32VFM4


    MKL05Z32VFM4


    4MKL25Z128VLK4


    KMKL26Z128VLH4

    H4

    MKL46Z256VLL4

    Typ. Operating Voltage

    3.3V3.3V3.3V3.3V3.3V

    Accelerometer

    3-axis, Digital output

    FreescaleMMA8451Q

    FreescaleMMA8451Q

    FreescaleMMA8451Q

    FreescaleFXOS8700CQ

    Freescale MMA8451Q

    Core

    Cortex-M0+

    Cortex-M0+

    Cortex-M0+

    Cortex-M0+

    Cortex-M0+

    MHz

    48

    48

    48

    48

    48

    Magnetometer3D, Digital output

    _

    _

    _

    Freescale FXOS8700CQ

    Freescale MAG3110

    Arduino R3 compatibility for expansion possibilities

    Y

    Y

    Y

    Y

    Y

    Capacitive touch slider

    2 electrodes controlled by SOFTW

    2 electrodes controlled by TSI

    2 electrodes controlled by TSI

    2 electrodes controlled by TSI

    2 electrodes controlled by TSI

    Easy access to MCU I/O

    Y

    Y

    Y

    Y

    Y

    IrDA

    _

    _

    _

    _

    _

    mbed Enabled

    _

    Yes

    Yes

    _

    Yes

    Flash/RAM/ FlexMem

    32KB Flash, 4KB RAM

    32KB Flash, 4KB RAM

    128KB Flash, 16KB RAM

    128KB Flash, 16KB RAM

    256KB Flash, 32KB RAM

    Segment LCD

    _

    _

    _

    _

    4x8 segments LCD module

    Sophisticated OpenSDA debug interface

    Mini USB connector

    Mini USB connector

    Mini USB connector

    Mini USB connector

    Mini USB connector

    Temperature Sensor

    _

    _

    _

    _

    _

    USB OTG FS Interface

    _

    _

    Mini USB connector

    Mini USB connector

    Mini USB connector

    User LED(s)

    Tri-color RGB

    Tri-color RGB

    Tri-color RGB

    Tri-color RGB

    1- Red, 1- Green

    Ambient Light Sensor

     

     

     

    EverlightALS-PT19-315C/L177/TR8

     

     

     

    3.3.2 FRDM-KE Series Board

     

     

    FRDM-KE02Z

    FRDM-KE02Z40M

    FRDM-KE04Z

    FRDM-KE06Z

    MCU Part No

    MKE02Z64VQH2

    MKE02Z64VQH4

    MKE04Z8VFK4

    MKE06Z128VLK4

    Typ. Operating Voltage

    5V

    5V

    5V

    5V

    Accelerometer3-axis, Digital output

    Freescale MMA8451Q

    Freescale MMA8451Q

    Freescale MMA8451Q

    Freescale MMA8451Q

    Core

    Cortex-M0+

    Cortex-M0+

    Cortex-M0+

    Cortex-M0+

    MHz

    20

    40

    48

    48

    Magnetometer3D, Digital output

    _

    _

    _

    _

    BLDC Motor control interface

    Motor control headers
    APMOTOR56F8000E

    Motor control headers
    APMOTOR56F8000E

    Motor control headers
    APMOTOR56F8000E

    Motor control headers
    APMOTOR56F8000E

    Arduino R3 compatibility for expansion possibilities

    Y

    Y

    Y

    Y

    Capacitive touch slider

    2 electrodes controlled by TSI

    2 electrodes controlled by TSI

    2 electrodes controlled by TSI

    2 electrodes controlled by TSI

    Easy access to MCU I/O

    Y

    Y

    Y

    Y

    IrDA

    Transmitter & Receiver EVERLIGHT PT12-21C/TR8 (RX)IR12-21C/TR8 (TX)

    Transmitter & Receiver EVERLIGHT PT12-21C/TR8 (RX)IR12-21C/TR8 (TX)

    Transmitter & Receiver EVERLIGHT PT12-21C/TR8 (RX)IR12-21C/TR8 (TX)

    Transmitter & Receiver EVERLIGHT PT12-21C/TR8 (RX)IR12-21C/TR8 (TX)

    mbed Enabled

    _

    _

    _

    _

    Flash/RAM/ FlexMem

    64KB Flash, 4KB RAM, 256B EEPROM

    64 KB flash,
    256B D-flash as EEPROM, 4 KB SRAM

    8 KB flash
    1 KB SRAM

    48MHz, 128KB Flash, 16KB SRAM

    Segment LCD

    _

    _

    _

    _

    Sophisticated OpenSDA debug interface

    Mini USB connector

    Mini USB connector

    Mini USB connector

    Mini USB connector

    Temperature Sensor

    10K Thermistor

    10K Thermistor

    _

    10K Thermistor

    USB OTG FS Interface

    _

    _

    _

    _

    User LED(s)

    Tri-color RGB

    Tri-color RGB

    Tri-color RGB

    Tri-color RGB

    Ambient Light Sensor

    _

    _

    _

    _

     

    3.3.3 FRDM-K Series Board


    FRDM-K20D50MFRDM-K64F
    MCU Part NoMK20DX128VLH5MK64FN1M0VLL12
    Typ. Operating Voltage3.3V3.3V
    Accelerometer3-axis, Digital outputFreescaleMMA8451QFXOS8700CQ
    CoreCortex-M4Cortex-M4
    MHz50120
    Magnetometer3D, Digital output_FXOS8700CQ
    Arduino R3 compatibility for expansion possibilitiesYY
    Capacitive touch slider2 electrodes controlled by TSI_
    Easy access to MCU I/OYY
    mbed Enabled_OpenSDAv2 / mbed
    Flash/RAM/ FlexMem128KB Flash, 16KB RAM, 32KB FlexNVM1 MB flash memory, 256 KB RAM
    Segment LCD__
    Sophisticated OpenSDA debug interfaceMini USB connector-OpenSDAMini USB connector
    OpenSDAv2 debug
    Temperature SensorROHMROHM
    BD1020HFV-TRBD1020HFV-TR
    USB OTG FS InterfaceMini USB connectorMini USB connector
    User LED(s)Tri-color RGBTri-color RGB
    Ambient Light SensorEverlight ALS-PT19-315C/L177/TR8

    HDR 1X2

    ALS-PT19-315C/L177/TR8

    RF module_

    Add-on nRF24L01+ Nordic
    2.4G Radio module


    4 Introduction to the OpenSDA interface

     

    OpenSDA is an open-standard serial and debug adapter. It bridges serial and debug communications between a USB host and an embedded target processor as shown . The hardware circuit is based on a Freescale Kinetis K20 family microcontroller (MCU) with 128 KB of embedded flash and an integrated USB controller. OpenSDA features a mass storage device (MSD) bootloader, which provides a quick and easy mechanism for loading different OpenSDA Applications such as flash programmers, run-control debug interfaces, serial-to-USB converters, and more.

    1.JPG

     

    OpenSDA is managed by a Kinetis K20 MCU built on the ARM® Cortex™-M4 core. The Kinetis K20 includes an integrated USB controller that can operate at clock rates up to 50MHz. The OpenSDA circuit includes, at a minimum, a status LED and a pushbutton. The pushbutton asserts the Reset signal to the target processor, which could be a microcontroller, digital signal controller, or a microprocessor. It can also be used to place the OpenSDA circuit into Bootloader mode. SPI and GPIO signals provide an interface to either a JTAG or an SWD debug port on a target processor. Additionally, signal connections are available to implement a UART serial channel. The OpenSDA circuit receives power when plugged into a USB Host. In some designs, the OpenSDA circuit can also control the power supply of the target processor.

     

    New standard for embedded debug circuit supporting SWD and JTAG, it is Open hardware platform with proprietary and open-source software built on K20DX128 50MHz CM4. It provides serial channel and debug interface to the target MCU. Mass-storage bootloader used to load new applications into the OpenSDA

     

    4.1 OpenSDA MSD Bootloader

     

    Mass storage bootloader is Flash resident bootloader which is detected as Mass-storage USB device for which no custom host drivers required. We need to simple copy/paste or drag/drop interface for programming an Application binary file into the flash of the OpenSDA MCU.

    Bootloader runs if there is no Application installed or if forced by user (Reset button pressed during power on) or host-side software (method depending on Application implementation)

    1.JPG

     

    The OpenSDA MSD Bootloader provides a simple interface for loading an OpenSDA Application into the OpenSDA processor’s non-volatile memory. Only one OpenSDA Application may be resident at a time, and this application will be automatically run at startup unless Bootloader mode is selected.


    Two versions available:


    • Open-source, non-proprietary version:
      • Posted to online-repository (e.g. Google Code or github)
    • Closed-source, proprietary version:
      • Based on open-source code base
      • Only used on Freescale hardware
      • Will accept encrypted, proprietary binary
      • Allows for protection of proprietary software that can only run on official Freescale hardware

     

    4.2 OpenSDA Application Overview

     

    OpenSDA feature can be used in many ways which includes Mass Storage Programmer, P&E Multilink, Open Debug Standard, Cloud Computing Interface, Data Logging, and as customer’s application.

    1.JPG

     

     

    4.2.1 OpenSDA as Mass Storage Application

     

    MSD application is a closed source proprietary application that can be loaded using the controls the serial and debug interfaces to the target MCU. Mass-storage USB device providing a simple target MCU flash programmer and a virtual serial port (composite device)

     

    The MSD Bootloader appears in the host file system as a removable drive with a volume label of “BOOTLOADER”, An OpenSDA Application is loaded by simply dragging and dropping an OpenSDA Application file onto the BOOTLOADER drive, which implements a pseudo-FAT16 file system. OpenSDA Applications can be in S-record, raw binary file, or an encrypted .SDA file formats. Status information is provided through a text file named LASTSTAT.TXT.

                  1.JPG

     

    4.2.2 OpenSDA P&E Debug Application

     

    The P&E Debug Application is an OpenSDA Application that provides debugging and a virtual serial port all in one application. It provides a run-control debug interface that controls the JTAG or SWD debug interface to the target processor. It also provides a USB communications device class (CDC) interface that bridges serial communications between the USB Host and a UART serial interface on the target processor. Several integrated development environments support the P&E Debug Application including CodeWarrior for Microcontrollers (v10.3 and later), IAR Embedded Workbench (v6.40.3 and later), Keil MDK (v4.54 w/ P&E patch), as well as software from P&E Microcomputer Systems.

      1.JPG

    The P&E Debug Application is designed to debug the resident target processor in the OpenSDA system with limited support for off-board devices within the same processor family as the resident target processor. P&E’s Multilink and Tracelink hardware interfaces provide higher performance and additional debug features:


    4.2.3 OpenSDA Data Logging Application

     

    This application provides a simple, open-source OpenSDA application that fosters user community development and innovation by providing driver for virtual serial port communications to the target MCU with feature of basic debug control (SWD/JTAG) of the target MCU. Simple serial commands providing the ability to control and monitor the target processor.

    1.JPG

     

    4.2.4 OpenSDA + CMSIS-DAP

     

    • Freescale is collaborating with ARM on the definition of a new debug interface standard called CMSIS-DAP.
    • CMSIS-DAP will be one of the applications that runs on OpenSDA (Kinetis L and Vybrid boards are the first targets)
    • CMSIS-DAP will be a free application based on an open standard
    • mbed will utilize CMSIS-DAP to add debug capabilities (new to mbed)

    1.JPG

     

    4.3 MSD Flash Programmer

     

    The MSD Flash Programmer offers a very easy and convenient way to program applications into the flash of the target processor. Like the MSD Bootloader, the MSD Flash Programming Application emulates a FAT16 file system and enumerates as a mass-storage device. It appears as a removable drive in the host operating system with a volume label that matches the board name (for example, FRDM-KL25Z). Raw binary and Motorola S-Record files that are copied to the drive are programmed directly into the target memory device. This is most often the flash of the target microcontroller, but it could also be another memory device, such as a serial flash, depending on the specific implementation.

    1.JPG

    The MSD Flash Programmer is designed to program a specific target configuration. It does not support verification or configuration and is not recommended as a production programmer.

    The MSD Flash Programmer also provides a USB communications device class (CDC) interface that bridges serial communications between the USB Host and a UART serial interface on the target processor.

    Any freedom board comes with the MSD Flash Programmer OpenSDA Application preinstalled. Follow these instructions to run the OpenSDA Bootloader and update or change the installed OpenSDA Application

     

    4.3.1 Enter OpenSDA Bootloader Mode

     

    1. Unplug the USB cable if attached.
    2. Press and hold the Reset button (SW1).
    3. Plug in a USB cable (not included) between a USB host and the OpenSDA USB connector (labeled “SDA”).
    4. Release the Reset button

     

    A removable drive should now be visible in the host file system with a volume label of BOOTLOADER. You are now in OpenSDA Bootloader mode.

     

    4.3.2 Load an OpenSDA Application

     

    1. While in OpenSDA Bootloader mode, double-click SDA_INFO.HTML in the BOOTLOADER drive. A web browser will open the OpenSDA homepage containing the name and version of the installed Application. This information can also be read as text directly from SDA_INFO.HTML.
    2. Locate the OpenSDA Applications folder in the corresponding FRDM-KXXX Quick Start Package.
    3. Copy & paste or drag & drop the MSD Flash Programmer Application (for example MSD-FRDM KL46Z48M_Pemicro_v109 .SDA for the FRDM-KL46Z board) to the BOOTLOADER drive.
    4. Unplug the USB cable and plug it in again. The new OpenSDA Application should now be running and a FRDM-KL46Z drive should be visible in the host file system.

     

    You are now running the latest version of the MSD Flash Programmer. Use this same procedure to load other OpenSDA Applications.

     

    4.3.3 Load executables (Flash Programmer)

     

    1. Load the appropriate version of the MSD Flash Programmer application into the OpenSDA board
    2. Copy an S-record (commonly a file with .s19 or .srec extension) or a raw/flat binary file (commonly a file with a .bin extension) to the MSD removable drive with a volume label of the target hardware (for example, FRDM-KL46Z).
    3. If programming is successful, the embedded application executes automatically. Regardless, the contents of the LASTSTAT.TXT file are updated with the latest status information.

     

    The OpenSDA LED indicator is used by the MSD Bootloader and the standard OpenSDA Applications to provide mode and status information.


    In Bootloader mode running normally with no error condition LED will Blinking: 500ms on, 500ms off

     

    In application mode running normally with no USB activity LED are ON

    In application mode with USB activity LED are blinking


    5  Complementary Development Board: Freescale Tower System

     

    A modular development platform for 8/16/32-bit MCUs & MPUs


    • Quickly combine Tower Modules to build a prototype of your application
    • Modules sold individually or in kits
    • Open Source: Build your own Tower Module to integrate your IP
    • Cost-optimized hardware
    • Software support from Freescale and Third Parties
    • Growing community of Third Party hardware support
    • On-line community: www.towergeeks.org

    1.JPG

    Build Your System in 3 steps or less

    • Choose a Processor (MCU/MPU) Module

    1.JPG

    • Choose Peripheral Modules and Tower Plug-Ins (TWRPIs)

    1.JPG

    • Up to 3 peripheral modules
    • One additional side-mounting peripheral modules
    • Multiple TWRPIs
    • Connect each module to the Elevator Boards

    1.JPG

    6  Freescale’s Microcontroller Enablement

     

    ARM processors power hardware development platforms with a wide range of design complexity levels. From simple microcontroller boards to very advanced multi-core solutions, most ARM-based development boards are manufactured by a variety of ARM partners and sold through distributors. Freescale enablement consists of software, Hardware, Middleware and supporting tools to enable user to develop their product.  Below are the tools supported for Kinetis family MCU.

    1.JPG

     

    6.1 Software Development Tools

     

    Freescale CodeWarrior, Freescale Freemaster, Atollic, Hitex, IAR Systems, Keil (ARM), Rowley Associates, Code Re, ARM GCC Embedded

     

    These are primary IDEs to promote with Kinetis family MCU:

     

    1. FREESCALE CodeWarrior v10.6:
         Available now

                         Free Version: 30 Days free trial Evaluation Edition, 128KB Special Edition

    2. FREESCALE Kinetis Design Studio v2.0 (KDS)
        Available in October 2014
        100% Free toolchain

    3. IAR EWARM :
        Available now

       Free Version : 30 Days free trial, 16KB KickStart

    4. KEIL MDK :
        Available now

        Free Version : 30 Days free trial, 32KB MDK-Lite

    5. EMPROG CrossWorks for ARM
        Available now
        Free Version : 30 Days free trial

                     6. ATOLLIC TrueStudio
                        Free Version: 30 Days free trial, 8KB Lite Version

                     7. Rowley Crossworks

            Free version available

                     8. mbed
                         Available now for FRDM-KL05Z, FRDM-KL25Z, FRDM-KL46Z, FRDM-K64F

                         Free online toolchain without debug capabilities

                     9. Coocox
                          Free Toolchain: coocox.org/freescale

                     10. GCC ARM Embedded

              Free command line compiler: launchpad.net

     

    6.1.1 Processor Expert Software

     

    Microcontroller Driver Suite v10.4 is a software management system that generates C code to create, configure, optimize, migrate and deliver software components, such as peripheral drivers, for Kinetis and ColdFire+ processors. The driver suite is delivered and installed as a comprehensive product with the Eclipse 4.2 (Juno) IDE. It is also available as an Eclipse plug-in for existing Eclipse 3.7 (Indigo) and Eclipse 4.2 (Juno) installations. The driver suite does not include a compiler or linker. You merge the generated code into a build system. This functionality is integrated into the CodeWarrior tools. The driver suite provides the same kind of support for our ecosystem tools partners. This extends Processor Expert software functionality to non-CodeWarrior IDE users for the supported platforms.


    Features of Processor Expert:

    • Extensive and comprehensive knowledgebase of all supported silicon encapsulating all pins, registers, etc.
    • Silicon resource conflicts flagged at design time, allowing early correction
    • Simple creation of optimized peripheral drivers without reading silicon documentation
    • Easy integration of an RTOS with peripheral drivers using RTOS adaptor component
    • Enables straightforward migration to new hardware

     

    New Hardware Configuration Perspective

    1.JPG

    • Silicon configuration, and so much more
    • A software system to
      • Create…
      • Configure…
      • Optimize…
      • Migrate…
      • Deliver…
    • Reusable components
      • Drivers and libraries
    • For Freescale silicon
      • Kinetis, S08, S12, ColdFire, DSC …
    • Integrated in CodeWarrior MCU support is also available stand-alone as the Microcontroller Driver Suite


    Design new Software in just 7 Steps!!

    1.JPG

     

    6.1.2 Freescale CodeWarrior Development Studio

     

    Freescale’s CodeWarrior for Microcontrollers v10.6 integrates the development tools for the ColdFire®, ColdFire+, DSC, Kinetis, Qorivva, RS08, S08 and S12Z architectures into a single product based on the Eclipse open development platform. The modular installer provided with the tools, however, allows you to select and install only the Freescale architecture support you need for your application development.

    1.JPG

    Features of CodeWarrior:


    • Eclipse IDE 4.2.1 (Juno) and CDT 8.1.1
    • Unlimited assembler
    • C/C++ compiler and debugger (restrictions based on suite)
    • Integrated flash programmer
    • Full-chip simulation for DSC, RS08 and S08 derivatives
    • Processor Expert software and components
    • Processor Expert component development environment(restrictions based on suite)
    • Kernel-aware debug (Professional Suite only)

    New features:

    • 64-bit 'long long' and 64-bit floating point support for S12Z devices
    • Intrinsic support for Square Root and Hardware Divide commands for the Kinetis V Series
    • Optional New Component Inspector available with Processor Expert
    • P&E Cyclone Universal [FX] support

    1.jpg

     

     

    6.1.3  IAR Embedded Workbench

     

    The IAR Embedded Workbench® is an integrated development environment with a C/C++ compiler for building and debugging ARM processor-based embedded applications.

    2.jpg

     

    • Reliable, Powerful and Easy to Use
    • The most widely used C/C++ tool chain for ARM MCUs
    • Support for Kinetis K-series (10/20/30/40/50/60/70), Kinetis L-series, i.MX, ColdFire+ and ColdFire
    • Advanced trace debug functionality
      • Power debugging - optimize for power consumption with power profiling
      • Timeline shows graphical representations of power consumption, call stack,
        variable values and interrupt activity over time
      • Function profiling and code coverage
      • ETM and SWO trace support
    • Freescale MQX™ RTOS integration
    • Ready-made project templates
    • Project examples for the Freescale Tower system
    • Professional technical support organization

     

    6.1.4 Keil IDE Microcontroller Development Kit for ARM (MDK-ARM)

     

    The ARM Keil™ Microcontroller Development Kit (MDK-ARM) is the recommended software solution for students working with most of the Cortex-M, ARM7, or ARM9 processor-based MCU devices. It features the industry-standard compiler from ARM, the Keil μVision® IDE, and sophisticated debug and data trace capabilities. A free evaluation of the MDKARM is available from the Keil website which features everything from the full commercial version with a 32 KByte object code/data limit. For educational purposes and simple experimentation with ARM processors (even without the need for hardware), the MDKARM evaluation is ideal.

     

    • Tailored to ARM Cortex-M devices
      • Complete support of Kinetis family of devices
      • Optimized Compiler, IDE, Debugger, Debug/Trace Adapters and Middleware
      • Support advanced Cortex-M and CoreSight technologies
    • Enable developers to:
      • Start projects faster
        • Device Database provides tool setup, header files,
          start-up code, flash algorithm, etc.
    • Use Middleware Libraries for Kinetis K60 & K70
      • Ethernet, USB Host & Device, Flash File system and GUI
    • Write efficient DSP code
      • ARM Compiler optimized for Cortex-M4 SIMD instruction set
    • Verify and optimize software
      • ULINKpro with Streaming Trace provides
        Code Coverage and Performance Analyzer

      1.jpg

    • Leading supplier of MCU development tools

                - ANSI C/C++ compilers, Debuggers and Simulation                        

                -  Middleware components

    • Extensive Device Database

              Directory of over 700 supported ARM MCUs

    • Established support

     

    MDK-ARM Versions:


    • MDK-STANDARD-FREESCALE (1year license with no code limits): $745 Supports any Cortex-M-based Kinetis Family device

     

    • MDK-LITE (32K Code Limited): FREE

     

    • MDK-STANDARD (T) (1 Year Licence): $1.958

     

    • MDK-BASIC (B) (256KB limit): $2.695

     

    • MDK-STANDARD: $4.895

     

    • MDK-PROFESSIONAL: $9.995
      (30-day evaluations and floating Options available for most license types)

     

     

    6.2 mbed Development Tools

     

    The mbed platform provides free software libraries, hardware designs and online tools for professional rapid prototyping of products based on ARM microcontrollers. The platform includes a standards-based C/C++ SDK, a microcontroller HDK and supported development boards, an online compiler and online developer collaboration tools.

    1.JPG

     

    6.2.1 mbed SDK


    The mbed Software Development Kit (SDK) is a C/C++ microcontroller software platform relied upon by tens of thousands of developers to build projects fast. We've worried about creating and testing startup code, C runtime, libraries and peripheral APIs, so you can worry about coding the smarts of your next product.

    The SDK is licensed under the permissive Apache 2.0 licence, so you can use it in both commercial and personal projects with confidence.

    1.JPG

    The mbed SDK has been designed to provide enough hardware abstraction to be intuitive and concise, yet powerful enough to build complex projects. It is built on the low-level ARM CMSIS APIs, allowing you to code down to the metal if needed. In addition to RTOS, USB and Networking libraries, a cookbook of hundreds of reusable peripheral and module libraries have been built on top of the SDK by the mbed Developer Community.

    The mbed SDK gives you an API-driven approach to microcontroller coding. You can code using meaningful abstract objects and API calls, so you don't need to learn the microcontroller hardware details to get going. There is even a "Hello World!" example for every peripheral, just to get you started before you know it.


    6.2.2 mbed HDK


    The mbed Hardware Development Kit (HDK) provides full microcontroller sub-system design files and firmware for building development boards and custom products that benefit from the native support of the mbed SDK and free mbed Online Compiler and mbed Developer Platform.

    1.JPG

     

    The HDK specifies all support components and circuits including the mbed Onboard Interface design that provides simple USB drag-n-drop programming and CMSIS-DAP debug interface for the target microcontroller.

    Development boards that are already based on the HDK are the quickest way to get started with the mbed platform. We manufacture official mbed Microcontroller modules that are specifically optimised for flexible rapid prototyping, and are available from distributors worldwide. Our partners are now also creating mbed-enabled hardware such as ultra low-cost ARM evaluation boards in the popular Arduino form-factor.

     

    6.2.3 Benefits of the mbed


    There are various benefits to building a custom design onto of the mbed HDK. The ready made schematics are a great short cut, so you can get started on all the things that make your design, without worrying if you've correctly implemented all the "necessary bits" of the design. The mbed HDK incorporates the CMSIS-DAP interface. This provides USB drag and drop programming, CMSIS-DAP debugging and USB serial communication. The mbed SDK supports each of the exact configurations of HDK designs, and libraries that have been written to the APIs in the mbed SDK are highly reusable. Lastly, the mbed community has developed a wealth of libraries, applications and code examples using the SDK/HDK, and this active community offers a lot of opportunities for support and even hiring in required skills.


     

    6.3 Hardware Development Tools

     

    Freescale Tower System, Freescale Freedom Platform, Hitex, IAR Systems, Keil (ARM), P&E Micro Systems, SEGGER

     

    1.jpg


    6.3.1  Segger Tools

    J-link

    1.JPG

    • Support IDEs such as IAR, Keil, Code Soucery, CodeWarrior and more
    • Supports JTAG, SWD, SWV Interface
    • Supported CPUs: Any ARM7,9,11, Cortex-M0, M1, M3, M4, R4
    • Flash breakpoints allow the user to set an unlimited number of software breakpoints when debugging in flash memory.
    • Performance Comparison: (Download into RAM):
    • Embedded Trace Buffer (ETB) support


    Addition Software    

    1.JPG

    • J-Link GDB Server – a remote server for the GDB.
    • J-Flash (PC software ) - program your Flash EEPROM devices via the On-Chip Debug connector (JTAG) on your target system.

                    

    High Performance Flash Programmer

     

    • Segger Flasher

     

    Product Cost Peak download  into RAM (KByte/sec) Added Features
    Segger J-Link Ultra $648 1440 JTAG speed up to 25MHz
    Hi-Speed USB
    On Board FPGA
    Segger J-Link $299 720 JTAG speed up to 12MHZ
    Segger J-Link Lite In KIT 280
    Abatron BDI2000 340
    ARM RealView Multi-ICE


    6.3.2 P&E Micro Tools

     

    Multilink Universal

     

    • Support IDEs such as CodeWarrior and P&E Software
    • Supported CPUs: Any Freescale ColdFire, Power, 8bit, kinetis, DSC
    • 1.6 – 5.5 V
    • Supports JTAG, SWD Interface

     

    Product

    Cost

    JTAG speed of

    Added Features

    Open Source JTAG

    Free

    250 KHz

    Built-in to Tower

    Universal Multilink

    $119

    1 MHz

    Support Many architectures

    Universal Multilink FX

    $399

    10 MHz

    Data Monitor, High Speed

    Tracelink

    (Q2-2012)

    $999

    30 MHz

    External Trace, Very High Speed

     

    Stand alone programmer & debug

    1.JPG

    • Cyclone Universal Q2/Q3 2011
    • Cyclone Universal FX Q2/Q3 2011

     

    6.3.3 KEIL Tools

     

    ULINK Debug and Trace Units

    1.jpg

    ULINK2: Debug + Serial Wire Trace

    • Flash Programming + Run-Control
    • Memory + Breakpoint (access while running)
    • Serial Wire Trace Capturing up to 1Mbit/sec (UART mode)

      

    ULINKpro: adds ETM + Streaming Trace

     

        1.jpg

    • Cortex-M processors running up to 200MHz
      • 50MHz JTAG clock speed
      • Serial Wire Trace Capturing up to 100Mbit/sec
        (Manchester Mode)
      • ETM Trace Capturing up to 800Mbit/sec
    • Virtually unlimited Trace Buffer
      • Streaming Trace allows complete Code Coverage and Performance Analysis
    • Full supporting of the Micro Trace Buffer in Kinetis L Cortex-M0+ based devices

     

    6.4 Operating Systems

     

    Freescale MQX™, Embedded Access, FreeRTOS, Keil (ARM), Micrium, SEGGER


    Freescale MQX Software Solutions Summary

    • RTOS (Full priority-based, pre-emptive scheduler)
    • Real-time TCP/IP Communication Suite (RTCS)
    • TCP/IP, FTP, Telnet, DHCP, SNMP etc..
    • USB Host - HID, MASS, HUB
    • USB Device - HID, MASS, CDC
    • MS-DOS File System (MFS )
    • BSP I/O Driver: CAN, UART etc…
    • HTTP Web server

    Benefits

    • Full production source code  with silicon
    • Business-friendly licensing model that lets developers keep their source modifications
    • Small, configurable footprint
    • Integrated stacks (TCP/IP, USB, etc.)
    • Customers focus on their application, not drivers, porting work, or integration work

     

    7 Basic Exercise on Freedom Board

     

    This section brings you a hands-on exercise working on Freedom board using Processor expert and mbed software development tools.

     

    User must download the Quick Start Package for the Out Of the Box Experience and the Sample Code Package to go further with his evaluations

     

    7.1 Freescale Processor Expert - Make FRDM-KL25Z RGB Blink Exercise

     

    1. Enter FRDM-KL25Z with P&E OpenSDA Debug mode (refer to OpenSDA section)

     

    2. Import the Components:     LED: Universal LED driver

                                Wait: Universal waiting functions

    3. Create a new Project:

        

    File > New > Bareboard Project

      • Select MKL25Z128 device      
      • Select OpenSDA debug connection     
      • Select Processor Expert Option    

    1.JPG

         

    4. Add and Set up the components


    • Add the LED component to the project 3 times: red, blue and green color.


    • Change the settings in the Component Inspector for the three LED’s:
      - change Component name: LEDR, LEDG and LEDB for the three colors
      - specify a Field Name: same name I used in the LDD

     

    • According to the FRDM-KL25Z Schematics, LEDs are connected to following pins: Red: PTB18, Green: PTB19, Blue: PTD1

     

    - Repeat those steps for LEDG and LEDB.

     

    • Add the Wait Component to the project to busy wait between the LED toggling

    1.JPG


    5. Generate Code


      1.jpg

     

    6. Add the Main Code

    Application main() is inside ProcessorExpert.c, where add my LED demo code:


    for(;;) {
     WAIT1_Waitms(100);
     LEDR_Neg();
     WAIT1_Waitms(200);
     LEDG_Neg();
     WAIT1_Waitms(400);
     LEDB_Neg();
     }
    
    
    



    7. Build the Project and Download and Debug

    1.JPG

     

     

    7.2 Exercise on mbed - Blinky, Touch Sensor and Accelerometer exercises

     

    1. Create/Log-In with your mbed account

     

    Connect your microcontroller to a PC, After a few seconds of activity, the PC will recognise the mbed Microcontroller as a standard USB drive

    1.jpg

    Click the MBED.HTM link to get logged in. Go to the new USB Drive, and click MBED.HTM to open it in a web browser.

     

    If you do not have an mbed account, choose "Signup", and create your mbed Account. Otherwise, log in with your normal username and password. This will give you access to the website, tools, libraries and documentation.

     

    2. Downloading a program


    Start the FRDM-KL25Z with the OpenSDA mbed application and check drag'n dropping the HelloWorld_KL25Z.bin precompiled project example available at http://mbed.org/handbook/mbed-FRDM-KL25Z-Downloading and press the reset button (blue LED should flash).

     

    3 Create a project with the mbed compiler

     

    • Open the mbed Compiler (top-right of the page)
    • Create a New Program (Right-click on My Programs, and select New Program)

    1.jpg 

    View the default program source code (main.cpp by default HelloWorld_KL25Z source code)

     

    Click on the "main.cpp" file in your new program to open it in the file editor window. This is the main source code file in your program, and by default contains a simple program already.


    1.jpg

                                                                                                              

     

    • Compile and Download the Program

     

    To compile the program, click the Compile button in the toolbar. This will compile all the program source code files within the program folder to create a binary program.

       1.jpg                                                               

    • After a successful compile, you will get a "Success!" message in the compiler output and the download dialog will pop up. Save it to the location of the mbed Microcontroller drive, and then hit reset on the microcontroller to start it running!
    • If there are errors, they will show up in the "Compiler Output" window, and will need to be fixed!

     

    4. Choose a project example featuring the RGB LED, the accelerometer or the touch sensor


    mbed FRDM-KL25Z - Hello World!

    1.jpg

    Touch Sensor - Hello World!

    1.jpg

    Accelerometer - Hello World!

     

    1.jpg

     

    References:

     

    1. http://www.freescale.com/

    2. http://www.arm.com/

    3. http://infocenter.arm.com/help/index.jsp

    4. http://mbed.org/teams/Freescale/

    5. http://www.pemicro.com/opensda/