Version 2

    For all other information and technical documents on the Raspberry Pi Model B+ 512MB please refer to Raspberry Pi Model B+


    B+ overhead image - smaller.jpgTo determine the board revision, either directly at the Raspberry Pi command prompt, or via a terminal session, type the following command:

    cat /proc/cpuinfo

    Model and revisionCode(s)
    Model B Revision 1.02
    Model B Revision 1.0 + ECN0001 (no fuses, D14 removed)3
    Model B Revision 2.04, 5, 6
    Model B Revision 2.0 (512 MB)13, 14, 15
    Model B+ Revision 1.27

    For Applications Which Rely on the GPIO Header
    There has been a change to the GPIO pin out of the B+ to the Model B, to add I2C ID EEPROM support and to add 9 additional GPIO pins. Users wishing to produce portable GPIO code should either avoid using the ID EEPROM, or add code to check the board revision and use this result to drive the correct pins appropriately. With the removal of the P5 and P2 site(s) and redesign of the board, the once 26 pin GPIO block has been extended to 40 pin, the added 9 accessible GPIO are named:

    • GPIO05, GPIO06
    • GPIO12, GPIO13
    • GPIO16, GPIO19
    • GPIO20, GPIO21, GPIO26

    Along with three additional Ground pins in the same extended block.


    USB Output Power / Ports

    The USB Hub and Ethernet controller has been changed from the SMSC LAN9512-JZXSMSC LAN9512-JZX to the SMSC LAN9513-JZXSMSC LAN9513-JZX , this increases the supported USB ports to 4 downstream, one upstream.


    ID EEPROM Support
    Two GPIO pins have been added to allow an extension board to communicate over I2C to identify itself and configure the GPIO pins accordingly


    Mounting Holes
    Four 2.5mm (drilled 2.9mm for M2.5 screw) non plated mounting holes have been provided. Positions of of the holes are in each corner of the PCB where possible and an on-board connector is not soldered.

    Warning: If used to permanently mount the PCB – do not over tighten screws or drill out to fit larger screws, as this will lead to irreversible PCB damage.



    These have been moved to the opposite side of the board, next to the GPIO and consolidated into an ACT (activity) and PWR (power) LEDs. The ACT LED reflects SD Card access only.

    Composite RCA / Audio Jack Changes

    The composite video phono/ RCA socket has now been integrated into the 3.5mm audio jack. To use it requires a 4 pole 3.5mm plug which breaks out the video and/or breaks out the audio into the required sockets/plugs.


    Material Source and Accuracy

    The materials for this document have been sourced from observations of a physical Raspberry Pi B+ compared to the latest Raspberry Pi Model B and relevant technical documentation for parts on each.

    Product Recommendation:

    Raspberry Pi Model B+Raspberry Pi Model B+

    Raspberry Pi Model B+ with 8GB microSD CardRaspberry Pi Model B+ with 8GB microSD Card