Version 4

    Protocol information for Tenma 72-2550 and Tenma 72-2535

    Please check following, if usb is not working.

    Please test the software if USB works well or not?

     

    One more thing to be confirmed with the customer as follows:

     

    After you send commands, there will be a beep. Even there is an error; if you confirm USB works well, please check if there is something wrong with the command, for example, there should not be carriage returns or terminator behind the command *IDN?

     

    Therefore, if there is carriage returns or terminator after you type the command, the error will be caused.

    Q;TENMA 72-2550 can be controlled with Matlab software?

    A:Yes, TENMA 72-2550 can be controlled with Matlab software, as confirmed by supplier.