Version 11
    MCU/MPU/DSP > Emulation & Debugging > Debugging Accessories >
    • J-Link 6-pin Adapter
    • J-Link 6-pin Adapter
    Technical Docs
    Product Brief/Fact sheet

    Overview

    The J-Link 6-pin Adapter has been designed to connect J-Link to a PCB which does not come with a mating connector or programming header. The designed pattern with 3 locating pins ensures, that the adapter can only be connected in one way. The 6-pin Adapter allows manufacturers to save costs and space on their PCBs since there is no need to provide the PCB with additional connectors. It adapts from the standard 20-pin 0.1'' J-Link connector to a 6-pin needle connector.

    J-Link 6-pin Adapter is compatible to J-Link BASE, J-Link PRO, J-Link ULTRA , J-Link EDU, Flasher ARM, Flasher RX, Flasher PPC and Flasher Portable.

    Pinout: the three locating pins ensure, that the adapter can not be connected to the PCB the wrong way. Moreover, the two "legs" on each side of the connector guarantee a stable and secure contact between pins and the PCB.

    Note: If JTAG support is required, use the J-Link Needle Adapter instead, since the 6-pin Adapter does not provide enough pins for JTAG.

    Features

    • No additional connector required on your PCB
    • Very small footprint - even smaller than the footprint of the (10-pin) J-Link Needle Adapter.
    • High reliability spring pins for secure connections
    • Designed with 3 locating pins, so the adapter can not be connected the wrong way

    Ships With

    • Adapter

    Blog Posts

    Discussions