Version 38

     

    Connectors I

    What are Connectors?

    Sponsored by

    1. Introduction2. Objective3. Definition4. Function
    5. The Anatomy of a Connector6. Types of Connectors Parts UsedTest Your Knowledge

    Vote for the next Learning Module subject!

    1. Introduction

    A connector system performs the all important role of interconnecting a product’s printed circuit boards (PCBs), power supplies, control panels and other sub-assemblies. While connectors may appear to play a passive role in an end-product’s performance, in reality, they influence the safety, reliability, and ease-of-maintenance of a product. To select the ideal type of connector for a specific design or application, a design engineer can benefit from a basic knowledge of connector technology.

     

    2. Objective

    The objective of this learning module is to provide you with the essentials of connector technology. You will first learn the purpose, function, and components of a connector.  In the later sections, you will gain a deeper understanding of the types, materials, features, and applications of PCB, Card/Slot and I/O connectors.

    Upon completion of this module, you will be able to:

    Define what connectors are and the purpose they serve;

    Discuss the primary functions of a connector;

    Describe the anatomy of a connector;

    Identify the most common types of connectors.

     

    3. DefinitionBack to Top

    What is a connector? Is a connector simply a means to connect two electrical points of a circuit, or is its purpose broader in scope? To understand the purpose of a connector, let us consider a jumper wire. Is a typical jumper wire – one that connects circuit components together on a prototyping breadboard – a connector?

    A jumper wire can connect two points of a circuit together, but lacks the mechanical integrity or environmental protection required in an end-product that is subjected to vibrations, abuse, corrosion or water sprays. In this respect, a connector provides more than a means of electrical connection, but should offer a durable mechanical or mating connection as well. So, maybe a jumper wire falls short as a connector.

    If a jumper wire isn’t a connector, then what exactly is? Let’s look at the definition of connector to find out:

    A connector is a device that is capable of connecting two circuit points, signals, or sub-systems with electrical integrity, mechanical durability, environmental protection and safety.

    Electrical Integrity - when connectors mate two points of a circuit with a very low contact resistance and provide protection from electromagnetic interference (EMI) and/or electrostatic discharge (ESD).

    Mechanical Durability - when a connector can withstand vibrations or environmental abuse without causing a failure in electrical integrity.

    Environmental Protection - when a connector’s design meets the IP (Ingress Protection) ratings defined in the international standard EN/IEC 60529 for preventing the ingress of water, dust, debris, and other contaminants that would otherwise interfere with the electrical integrity of the connection.

    Safety - when a connector is designed with features that eliminate personnel hazards, or the risk of fire, shock or electrocution.

     

    4. FunctionBack to Top

    To understand the function of a connector, let’s imagine for a moment a world without connectors. What would be the practical outcome of such a scenario?

    In such a world, all electronic components, sub-assemblies and electrical power would be connected by bare metal wiring. This means everything would be soldered, mechanically attached or twisted together. Doesn’t sound convenient, does it?

    It would be pretty hard to design products with high-circuit densities in a “No Connectors Allowed” world. Smart phones would probably be a lot bigger. And forget about portable charging stations or even your handy power adapter!

    What about electrical safety? Would a ”No Connectors Allowed” world be safer for a user? Could you safely connect the 120/230V mains to your home appliance without sparks flying?  (Probably not!) It’s time to go back to a world with connectors and learn the primary functions of a connector.

    The primary functions of a connector are:

    Quick Connection/Disconnection: Connectors provide a safe, quick and convenient means for connecting and disconnecting components, modules, systems and sub-assemblies during prototyping, manufacturing, installation, operation, or maintenance.

    Efficient Manufacturing: Connectors allow for the efficient production of products by eliminating many time-consuming tasks such as soldering.

    Easy Upgrades/Configurations: Connectors enable users to easily upgrade products or quickly configure new devices for these products.

    Eliminate Safety Hazards: Connectors shield users from hazardous currents that could pose a shock or electrocution hazard.

     

    5. The Anatomy of a ConnectorBack to Top

    There are many types and styles of connectors, yet they all share common characteristics. In this section, we will discuss the common components and features of a connector.

    The three main parts of a connector are:

    Housing

    Shell

    Contact

    - 5.1 Description of a Housing

    The housing is the component that provides a connector the mechanical durability, environmental protection and electrical insulation for the contact terminals.

    Connector housings have the following characteristics:

    Materials: Housings are made of stabilized, heat resistant, self-extinguishing thermoplastic material.

    Locking: Housings often have a locking tab to prevent connector housing halves from disconnecting and interrupting a circuit.

    Polarization: Housings are polarized to ensure the connector halves are mated correctly.

    Keying: Housings are keyed or arranged so only compatible contacts or circuits can be mated with one another.

    Environmental Protection: Housing often have shrouds or seals (depending upon the specifications of a connector) to prevent the ingress of dust, moisture, chemicals and other contaminants that could degrade the electrical integrity of the connection.

    Mounting: Housings can be mounted in a variety of ways, including PCB, panel, and wire-to-wire configurations.

    Fire Safety: High-performance composite materials help meet the low smoke, toxicity and flammability (UL 94V-0 rated) requirements of the application.

    - 5.2 Description of a Shell

    The shell encloses the connector housing thereby offers added strength and protection to the housing. Since shells are made of a nickel-plated, zinc alloy, they also offer excellent corrosion resistance.

    - 5.3 Description of Contacts and Terminals

    The contact consists of highly conductive material with very low resistance that allows the easy flow of electrical current through the two mated contacts.

    While the contact is the point where circuit current flows, the terminal is the means by which the contact is attached (or terminated) to a circuit’s conductor.  Often times the functions of both the contact and terminal are combined in one device. In this case, the word terminal and contact maybe used interchangeably.

    Contact terminals have the following characteristics:

    Materials: A variety of materials or alloys are used for electrical contacts and terminals based upon cost, electrical and thermal properties, resistance to oxidation (corrosion) and durability. The most common contact metals include: brass, phosphor bronze, and high copper alloy. Contacts are often plated for added strength, better conductivity and corrosion resistance. Plating materials include gold, silver nickel, tin, and palladium-nickel.

    Types: Contacts are constructed in the form of insertable/removable pins and sockets (informally referred to as “male” and “female,” respectively).

    Locking: Terminals often have locking wing tabs to securely hold the terminal in the connector’s housing.

    - 5.4 Description of Terminations

    Terminations are the manner by which the circuit’s conductors are attached to the connector’s contact terminals. The quality of the terminations is critical to the proper functioning of the circuits connected by a connector.

    Electrically sound terminations maintain a desirable low contact resistance at the point of connection. Conversely, terminations that are not electrically sound —opened, shorted, or high resistance points —can be detrimental to the proper functioning of the circuit.  This is a particular concern in high vibration environments (industrial machinery or automotive applications).

    The common types of terminations include:

     

    AMPLIMITE* HDP-20 Connectors with Solder Cup Contacts

    Solder Cup

    a type of termination where individual circuit wires are soldered on the connector’s “cup” terminals.

    TE Connectivity’s AMP  Wire-To-Board Connector, AMP CT Series, Crimp, Receptacle

    Crimping

    a type of termination that creates a secure and separable connection between the contacts and terminal wires.

    TE Connectivity’s AMP Circular Plastic Connector, Series 1, PCB Mount

    PCB Solder

    a type of termination where the contact terminals are soldered directly onto a PCB via through-holes.

    TE Connectivity 1735690-1  SAS Receptacle, Press-Fit

    Press Fit

    a type of termination where connector’s contact terminals are pressed through plated-through holes on a printed circuit board (PCB). The primary advantages include eliminating thermal stresses of PCB soldering and enabling higher density circuit applications.

    TE Connectivity’s AMP Mini USB, 2.0 Type A, Receptacle, Surface Mount

    Surface Mount

    a type of termination where the connector is mounted to the surface of a PCB and bonded to conductive pads via soldering.

    TE Connectivity’s AMP Wire-To-Board Connector, AMPMODU Series, IDC Plug

    Insulation Displacement Termination (IDC)

    a type of termination that connects insulated wire without requiring the pre-stripping of the insulation.

           

     

    6. Types of ConnectorsBack to Top

    There are a wide variety of connector-types used by design engineers and employed in prototypes and end-products. In general, connectors are grouped into the following main categories:

    PCB

    Card/Socket

    Input/Output

    - 6.1 PCB Connectors

     

    TE Connectivity 1744057-5 wire-to-board connector, Economy Power

    Wire to Board

    a type of connector that offers a separable connection between electronic sub-assemblies, PCBs, and rack/panels. Benefits include saving PCB space, enabling high-density connections, and providing design flexibility.

    TE Connectivity 3-2041390-9 ZIF Flexible Printed Circuit Connector

    Zero Insertion Force (ZIF)

    a type of wire-to-board connector that minimizes the insertion or extraction force, reducing contact wear. It is used with flat flex ribbon cable and has a mechanical arm that locks the contacts in place upon connection.

     

    TE Connectivity Board to Board Connector, Fine Pitch

    Board to Board

    a type of connector that connects one PCB to another in a stacking configuration. These connectors are for low-profile, tight-packaging or backplane connector applications.

    TE Connectivity Ribbon Cable Connectors

    Ribbon

    a type of connector used with flat ribbon cable to connect internal peripherals in computers, such as hard drives, CD drives and floppy drives. The ribbon connector is typically attached to the cable via insulation displacement rather than crimping or soldering, which allows for the mass termination of contacts.

    - 6.2 Card/Socket Connectors

     

    TE Connectivity AMP  1761465-31761465-3 Card Edge Connector Receptacle

    Card Edge

    a multi-circuit receptacle (female) that mates with the header (male) that's formed out of the traces that run to the edge of a PCB. They are primarily used in personal computers for connecting expansion cards, cartridges and computer memory to the system bus.

    TE Connectivity’s AMP IC & Component Socket, 800 Series, DIP

    Package to Board (IC Socket)

    a connector that provides a separable connection between an IC chip and a PCB via a through-hole soldered socket.

    TE Connectivity 1939870-1 SD Card Connector EMBOSS ASSY

    Memory Card

    a type of connector that connects microSD, SD, SIM, and/or MMC memory cards to portable or remote devices. They offer a variety of ejector types (e.g., push-push and push-pull) and provide polarization features to prevent improper card insertion.

    - 6.3 Input/Output Connectors

     

    TE Connectivity’s AMP Circular Plastic Connector Housing, Series 1, Panel Mount and 208473-1208473-1Metal-Shell Circular Plastic Connector Housing , Panel Mount

    Circular Plastic/Circular Metal

    a type of customizable, sealed or unsealed, commercial connector designed for power and signal connections and used in industrial, automotive, signal processing, power management and computer applications.  Both CPC and CMC connectors are made of stabilized, heat resistant, self-extinguishing thermoplastic material. CMC connectors have an additional metal shell to add greater strength and durability.

    TE Connectivity’s AMP  5749230-15749230-1 DIN Audio Video Connector PCB Mount

    S-Video

    an audio/visual connector used for transmitting Super-Video (S-Video) signals. The connector separates luminance and chrominance for a better picture and also to eliminate dot crawl.

    TE Connectivity’s AMP  5749768-15749768-1 Standard D Sub Connector Amplimite HD-22 Series DE-15

    Video Graphics Array (VGA)

    an analog, audio/visual connector for connecting PC displays. In graphics mode, the resolution is either 640 by 480 (with 16 colors) or 320 by 200 (with 256 colors). The original VGA standard has evolved over time to provide better resolution and more colors (e.g., SVGA and XGA).

    TE Connectivity 1734148-1  DVI Digital Video Interface Connector, Integrated Analog & Digital (DVI-I), PCB Mount

    Digital Visual Interface (DVI)

    a digital video connector used as an interface between computers, LCD monitors, projectors and other digital display equipment. It's based on the standard created by the Digital Display Working Group (DDWG) for converting analog signals into digital signals. It uses differential pairs for higher quality and better resolutions than VGA. It has RGB pins for backwards compatibility. It comes in a variety flavors, including DVI-D single link, DVI-D dual link, DVI-I single link, DVI-I dual link and DVI-A, analog.

     

    TE Connectivity  1746679-11746679-1 HDMI Connector Type A PCB Mount

    High-Definition Multimedia Interface (HDMI)

    an uncompressed, all-digital, audio/video interface/connector between any audio/video source, such as a set-top box, DVD player or A/V receiver, and an audio/video monitor such as a digital television (DTV). Unlike DVI, HDMI is both an audio and visual interface. HDMI has the capacity to support existing high-definition video formats such as 720p, 1080i, and 1080p, among others.

    TE Connectivity’s AMP  2040210-12040210-1 DisplayPort Digital Audio Connector Receptacle PCB Mount

    Display Port

    a digital display connector that employs packetized data transmission to connect a video source to an high definition (HD) video display. Developed by the Video Electronics Standards Association (VESA), it's an evolution of HDMI that supports higher resolutions as well as daisy-chaining. DisplayPort is backward compatible with VGA and DVI through the use of adapters.

    TE Connectivity’s AMP  3-1634222-23-1634222-2 Standard D Sub Connector AMPLIMITE HD-20 Series DE Receptacle 9

    D-subminiature (D-sub)

    a peripheral connector commonly used for connecting  RS-232RS-232 serial communication devices It contains a D-shaped metal shield that provides mechanical support ensures correct orientation and offers some level of EMI protection It is easy to work with and solder and its pin numbers are labeled on the connector But it is not as popular as in the past It also takes up a lot of space and has limited mounting options

    USB

    a connector based on the Universal Serial Bus specification, developed by the USB Implementers Forum, to standardize the connection of computer peripherals to personal computers, for both communicating and supplying electric power. The current types include:

     

    TE Connectivity 2129691-1  USB, 3.1 TYPE C

    USB Type-C

    the new standard plug or receptacle providing a multi-function, reversible, single cable solution for USB, power, and audio/video.

     

    TE Connectivity’s AMP 1981568-1 MICRO USB 2.0 TYPE B, RCPT, SMT

    Micro USB 2.0

    mostly used in mobile devices and is the smallest connector series in the USB family.

    TE Connectivity  1932258-11932258-1 USB 3.0 TYPE A RECEPTACLE SMTT

    USB 3.0

    support a 5Gbps data rate for fast syncing on the go—a 10x performance increase over USB 2.0.

    Coaxial

    an I/O connector that’s designed to work at radio frequencies in the multi-megahertz range.

    RF Products Overview (click on image to enlarge)

           

    All products are RoHS compliant Based on product type, design and manufacture to comply with standards: MiL-C-39012, Mil-STD-348, CECC, IEC for features and applications visit TE.com

    Modular Jack

    used to connect telephone systems or Ethernet networks. Common examples are RJ11 (telephone) and RJ45 (Ethernet) jacks.

    TE Connectivity’s AMP  2170668-12170668-1 CONN RJ45 CAT6

    *Trademark. TE ConnectivityTE ConnectivityTE Connectivity, TE connectivity (logo), and TE (logo) are trademarks. Other logos, product and/or company names may be trademarks of their respective owners.

     

    Shop our wide range of power, signal and data connectors, accessories and adapters.

    Shop NowShop Now Shop NowShop NowShop NowShop Now

     

    Test Your KnowledgeBack to Top

    Are you ready to demonstrate your Connectors knowledge? Then take a quick 15-question multiple choice quiz to see how much you've learned from this Essentials Connectors 1 module.

    You'll see your score at the end of the quiz. If you score 100%, you're on your way to earning your Connectors Skills 1 badge, and 100 points. To fulfil all the requirements for earning the badge, you will also need to post a feedback comment on this Essentials Connectors 1 page to let us know what you thought of the module, and bookmark this page so you’re the first to hear when Module 2 is published.

     

    1) A connector has which of the following characteristics?





     

    2) A jumper wire is not a connector. True or false?


     

    3) Connectors provide a safe, quick and convenient means for connecting or disconnecting circuit components during:





     

    4) A contact pin is commonly referred to as the ________ end and a contact socket is commonly referred to as the ________ end.





     

    5) Which of the following is NOT a main part of a connector?





     

    6) Unlike DVI, which is only a (an) _______ interface, HDMI is a (an) _____ and _____ interface.





     

    7) Why are connector-housings polarized?





     

    8) Which of the following is NOT a primary function of a connector?





     

    9) Which of the following is NOT used as an electrical contact material?





     

    10) What is the benefit of plating an electrical contact?





     

    11) The primary advantages of Press Fit terminations include the elimination thermal stresses caused by PCB soldering and the enablement of high density circuit applications. True or false?


     

    12) What type of wire termination does NOT require the pre-stripping of wire insulation?





     

    13) What type of connector connects one PCB to another in a stacking configuration?





     

    14) A DisplayPort connector interface is backward compatible with...





     

    15) What is a primary benefit of a USB Type "C" connector?





    Alas, you didn't quite meet the grade. You only got %. Have another look through the course, and try again.
    You nailed it, and scored %! Complete the quiz, bookmark this page and leave your feedback in the comments to earn the Connector Skills I badge, and bag 100 points!