Version 2
    Raspberry Pi > Development Platforms and Kits > Daughter / Add-on boards >
    • Gyroscope – angular rate sensor: ±245/500/2000dps
    • Accelerometer - Linear acceleration sensor: ±-2/4/8/16 g
    • Magnetometer - Magnetic Sensor: ± 4/8/12/16 gauss
    • Barometer: 260 – 1260 hPa absolute range
    • Temperature sensor: to ± 2 degC in the 0-65 degC
    • Relative Humidity sensor
    • 8x8 LED matrix display
    • Small 5 button joystick
    The Raspberry Pi Sense HAT is attached on top of the Raspberry Pi via the 40 GPIO pins. The Sense HAT has several integrated circuit based sensors that can be used for many different types of experiments, applications, and even games.

    The Sense HAT has an 8×8 RGB LED matrix, a five-button joystick and includes the following sensors: Gyroscope, Accelerometer, Magnetometer, Temperature, Barometric pressure, Humidity.

    Applications:
    • Consumer Electronics
    • Embedded Design & Development
    • Hobby & Education
    • Sensing & Instrumentation
    • Raspberry Pi Sense HAT is being used in conjunction with the Raspberry Pi Foundation to perform science experiments aboard the International Space Station (ISS)
    • Raspberry Pi Sense HAT
            
    TypeDocument
    Quick Start GuideGetting Started with the Sense HAT (.html)