Version 3
    MCU/MPU/DSP > Development Platforms & Kits >
    Moto Mods Audio Personality Card
    The Audio Personality Card provides an example of a Moto Mod™ with audio output. The included speaker uses a Class-D amplifier that is controlled using a I2S interface.

     

    This is the hardware companion to the Moto Mods Development Kit found at developer.motorola.com

    Overview

    The Audio Personality Card provides an example of a Moto Mod™ with audio output. The included speaker uses a Class-D amplifier that is controlled using a I2S interface. This card plugs into the 80 pin connector that comes with the Reference Moto Mod. While attached, this card will replace the internal Moto Z loudspeaker. Android audio routing rules remain unchanged, so no 3rd party application is required.

    As a developer, you can use this as a reference when designing and building your own Moto Mod prototype that needs it’s own audio connection. The source code for both the Moto Mod firmware and companion Android application is also available for your review and use.

    Features

    • Provides an example of a Moto Mod™ with audio output
    • Plugs into the 80 pin connector that comes with the Reference Moto Mod

    Ships With

    • Audio Personality Card

    Blog Posts

    Discussions