Version 2
    MCU/MPU/DSP > Development Platforms & Kits > Daughter / Add-on boards >
    • Plug-In Kit for CC3120 Wireless Network Processor Booster Pack
    • Plug-In Kit for CC3120 Wireless Network Processor Booster Pack

    Overview

    The SimpleLink™ Wi-Fi® CC3120 wireless network processor provides users the flexibility to add Wi-Fi to any microcontroller (MCU). The CC3120 BoosterPack™ plug-in-module (CC3120BOOST) is a board which can easily be connected to TI’s MCU Launchpad kits (software examples provided for MSP-EXP432P401R); thus enabling rapid software development. The CC3120BOOST can be plugged into the Advanced Emulation BoosterPack (CC31xxEMUBOOST), and connected to a PC which emulates an MCU with SimpleLink Studio. Lastly, this kit can also be connected to any low-cost, low power MCU platform beyond TI’s Launchpad kits, through adapter boards.

    This kit comes in 3 configurations:
    1. CC3120BOOST + CC31XXEMUBOOST + MSP-EXP432P401R: run all software in the CC3120 software development kit (SDK) and develop on MSP432 MCU
    2. CC3120BOOST + CC31XXEMUBOOST: used for any CC3120 development
    3. CC3120BOOST: standalone CC3120 BoosterPack purchase option if you already have CC31XXEMUBOOST

    Features

    • CC3120 Wi-Fi Network Processor in QFN package
    • 2x20-pin stackable connectors (BoosterPack headers) to connect to TI LaunchPads and other BoosterPacks
    • On-board chip antenna with option for U.FL-based testing
    • Operates from alkaline batteries for low power designs
    • Wi-Fi CERTIFIED™ at the chip level by the Wi-Fi Alliance™

    Ships With

    • BoosterPack Plug-in Board
    • Micro USB Cable
    • Quick Start Guide

    Blog Posts

    Discussions