Version 2

     

    All 15 of the sponsored Challengers for the Pi Chef Design Challenge will receive for FREE the the kit detailed in the table below. 

    Our judges will choose 15 applicants to become sponsored challengers, and these challengers will receive the kit free of charge. If your application is not chosen to become a sponsored challenger, you can buy the kit from the link below and still be in the running to win!

     

    Raspberry Pi 3 Model B
    • Latest Full Size Model
    • Next Generation QUAD Core Broadcom BCM2837 64bit processor
    • Processor speed has increased from 900MHz on Pi 2 to 1.2Ghz
    • BCM43438 WiFi on board
    • Bluetooth Low Energy (BLE) on board
    • Upgraded switched power source up to 2.5 Amps (can now power even more powerful devices over USB ports)

     

    Once the sponsored Challengers receive their kit, they will then embark on their journey of designing an exciting and original project that uses the Raspberry Pi 3Raspberry Pi 3 Raspberry Pi 3Raspberry Pi 3 as the main ingredient to improve and expand their creativity in the kitchen. (NOTE: Even if you aren't a sponsored Challenger, you can still participate in the Design Challenge as long as you follow with the Terms and Conditions and integrate the Raspberry Pi 3 Model B into your design.)

     

    The deadline for project submissions is 1st December 2017.

     

    The Kit Buy Kit*Buy Kit*

    Raspberry Pi 3 Model B & 8MP Camera

    The Raspberry Pi 3 Model B builds upon the features of its predecessors with a new, faster processor on board to increase its speed. It also features WiFi and Bluetooth Low Energy capabilities to enhance the functionality and the ability to power more powerful devices over the USB ports.

    Buy NowBuy Now

    32GB Raspberry Pi NOOBS Operating System MicroSD Card

    A 32GB Micro SD card with the official Raspberry Pi NOOBS Software preinstalled on it. NOOBS stands for New Out Of Box Software which is the Operating System installer for the Raspberry Pi, this SD card includes installers for Raspbian, Windows IoT Core, OSMC, Open Elec and other disk partition tools.

    Buy NowBuy Now

    NXP Explore NFC Expansion Board

    The EXPLORE-NFC-WW is a high performance fully NFC compliant expansion board for the Raspberry Pi boards. This add on board includes everything needed to get started with RFID on the Raspberry Pi.  It operates in three NFC modes such as reader mode, peer to peer mode and card emulation mode. This board features an integrated high performance antenna and offers a flexible SPI interface.

    Buy NowBuy Now

    2.4" Touch Screen Hat

    The 4DPI-24-HAT is a 2.4-inch 320 x 240 Primary Display HAT for the Raspberry Pi, which plugs directly on top of a Raspberry Pi and displays the primary output which is normally sent to the HDMI or Composite output. It features an integrated Resistive Touch panel, enabling the 4DPi-24-HAT to function with the Raspberry Pi without the need for a mouse. It is designed to work with the Raspbian operating system. The 4DPi-24-HAT is powered directly off the Raspberry Pi's 40 way Header and the 2.4" touch screen allows effortless interaction with the Raspbian operating system.

    Buy NowBuy Now

    Piface Digital 2

    The PiFace Digital 2 is an add on board for Raspberry Pi that allows for connecting things that will influence the world around it. It includes components like relays, switches, digital and analogue I/O that will allow for connection to sensors, motors, lights etc and can be controlled by Raspberry Pi board. This add on board fits neatly above the Raspberry Pi and connects using the expansion connector. Ensure that all expansion pins are lined up with the holes on the PiFace Digital 2 socket.

    Buy NowBuy Now

    Sense Hat

    The Raspberry Pi Sense HAT is attached on top of the Raspberry Pi via the 40 GPIO pins. The Sense HAT has a stack of sensors that can be used for many different types of experiments, applications, and even games.  It features, Gyroscope, Accelerometer, Magnetometer, Barometer, Temperature Sensor, Relive Humidity Sensor, 8x8 LED Matrix and a 5 button joystick.

    Buy NowBuy Now

    International Raspberry Pi Power Supply

    Official Raspberry Pi power supply, ideal for use with any Raspberry Pi board. This power supply comes with 1.5m Micro USB lead and four changeable heads for use in the UK, Europe, Australia & US regions. It supports up to 2.5A of current which is plenty to power devices through the four USB ports on the board and save you from the often common brown-outs.

    Buy NowBuy Now

     

    Interested in Challenging the Challengers? You can do it as a non-sponsored Challenger! Here's How:

    All you need to do is get the low-cost Raspberry Pi 3Raspberry Pi 3 Raspberry Pi 3Raspberry Pi 3 and integrate it into your project, as well as post 10 blogs about your design journey in the Pi Chef space (tagging your blogs 'Pi Chef') and you'll be eligible to win the awesome prizes.