Version 4

    Arduino Home

    An Open-Source platform to create digital devices and interactive objects that sense and control physical devices.

    Arduino Tutorials
    Arduino Projects

     

    Arduino Create Now Supports the Deployment of Arduino Sketches on a Wide Range of Linux® IoT Devices and Single-Board Computers (SBC)

     

    The latest update of Arduino Create enables fast and easy development of IoT applications using the Arduino framework and libraries on a wide range of Linux® devices including Intel® SBCs, Raspberry Pi® and BeagleBone®

     

     

    Portland, USA – March 13, 2018: Today, at Embedded Linux Conference 2018, Arduino announced the expansion of the number of architectures supported by its Arduino Create platform (create.arduino.cc) for the development of IoT applications. With this new release, Arduino Create users can manage and program a wide range of popular Linux® single-board computers like the AAEON® UP² board, Raspberry Pi® and BeagleBone® as if they were regular Arduino boards. Multiple Arduino programs can run simultaneously on a Linux-based board and interact and communicate with each other, leveraging the capabilities provided by the new Arduino Connector. Moreover, IoT devices can be managed and updated remotely, independently from where they are located.

     

    To further simplify the user journey, Arduino has also developed a novel out-of-the-box experience for Raspberry Pi and BeagleBone boards, in addition to Intel®  SBCs, which enables anyone to set up a new device from scratch via the cloud without any previous knowledge by following an intuitive web-based wizard. Arduino plans to continue enriching and expanding the set of features of Arduino Create in the coming months.

     

    “With this release, Arduino extends its reach into edge computing, enabling anybody with Arduino programming experience to manage and develop complex multi-architecture IoT applications on gateways,” said Massimo Banzi, Arduino CTO. “This is an important step forward in democratizing access to the professional Internet of Things.”

     

    “At Arduino we want to empower anyone to be an active player in the digital world. Being able to run Arduino code and manage connected Linux devices is an important step in this direction, especially for IoT applications that need more computing power, like AI and computer vision,” added Fabio Violante, Arduino CEO.

     

    About Arduino

    Arduino is the world’s leading open-source hardware and software ecosystem. The company offers a range of hardware platforms, software tools, cloud services and documentation enabling anybody to be creative with technology. Arduino is a popular tool for IoT as well as one of the most successful tools for STEM/STEAM education.

     

    Millions of designers, engineers, students, developers and makers around the world are using Arduino to innovate in industrial applications, smart homes, farming, autonomous vehicles, music, games, toys, and more.

     

    For press inquiries please contact: press@arduino.cc

     

    PR Agency Contact:

    Janice Fenton

    Account Director

    Publitek

    1. janice.fenton@publitek.com

    +44 (0) 1225 470000