Version 7

    A Hack Like Heck Project Video

    Vote for this Video by using the Like or Share buttons

    Voting Instructions

    About Hack Like Heck
    Content Partner Program
    All Hack Like Heck Videos

     

     

    For the Hack Like Heck challenge, I designed a portable emulator that you can easily change the controller. So, if you are playing a NES game, you can use a NES controller. Or if you are playing a SNES game, then you can use a SNES controller and so on.  At the heart of it is a Raspberry Pi Zero W that drives a 5”, 800x480 LCD screen with 18 of its GPIO pins.  Other features include a speaker and headphone jack, a safe power off button and a USB power out so you can charge your cell phone.

     

    The parts that I used for this project include:

    • Raspberry Pi Zero W
    • 32GB SD Card
    • 5" 800x480 Display TFT Display from eBay
    • Adafruit TFT Friend
    • Battery Pack
    • Class D Amplifier
    • B503 50K Ohm Wheel Potentiometer
    • USB Hub
    • SNES Controller
    • NES Controller
    • Male Micro-USB connector
    • Female Micro-USB connector
    • The Speaker was cut out of an old birthday card that sang a song when you opened it.
    • The Power Switch, Off Button, LED, Resistors and Headphone jack I had laying around from previous projects.

     

    You can find links to the parts that I used on my github page.

     

    I have put all the .stl files on my Thingiverse page.

     

    Thanks for this opportunity to meet the Ben Heck Show crew and I had a lot of fun creating this video.

     

    P.S. I just saw the 12-18 min requirement. I easily had that much footage, but I cut a lot of it out to save on length. Now I wish wouldn't have. Oh well... I still think that it is an entertaining video.