Version 9

    Meet the Compute Module 3+ is the latest addition to the Raspberry Pi Compute Module range.

    Raspberry Pi Compute Module 3+ 8G, 16GB, 32GB

     

    For anyone already following the Raspberry Pi foundations work from a developers viewpoint will be very happy to hear that they have released a new Compute Module.
    Based on the same chip as Raspberry Pi 3 Model B+ Broadcom BCM2837B0, a 64-bit quad core processor running at 1.4GHz.

    For the uninitiated, the compute module range has all the brains and power of the Raspberry Pi but in a form factor that is optimized for being embedded into a design, for example the standard external USB, power and ethernet have been removed and broken out into the fin edge connector.  The Compute Module 3+ is priced lower than the average Pi and has a wider operating temperature range.

    In addition to the super fast processor the new Compute Model 3+ comes in three different onboard memory variants; 8GB, 16GB & 32GB, to suits every kind of industrial embedded design applications.

     

    But, what if you don't want onboard memory and your prototype has an SD card slot or other type of boot memory else where on its PCB?!?!... then we have you covered with the Compute Module 3+ Lite

    Compute Module 3+ Lite

    A Lite version of the Compute Module 3+ is also available.

    The CM3L brings the SD card interface to the Module pins so a user can wire this up to an eMMC or SD card of their choice.

     

    Raspberry Pi Compute Module3+ Lite

     

    Raspberry Pi Compute Module3+ Lite

    The Compute Module 3+ simplifies the design process engineers need to undertake when developing a System on Module (SoM) solution into their final product. Engineers do not need to concern themselves with the complexities of interfacing with the BCM2837B0 processor directly and instead can concentrate on designing the interfaces to their own IO board and their application software. This simplicity fosters rapid development.

     

    • Broadcom BCM2837B0, Cortex-A53 64-bit SoC @ 1.2GHz
    • 1Gbyte LPDDR2 SDRAM
    • Memory Options: 8 Gbytes, 16 Gbytes, 32 Gbytes eMMC Flash or None.
    • Multimedia: H.264, MPEG-4 decode (1080p30), H.264 encode (1080p30), OpenGL ES 1.1, 2.0 graphics
    • SD card support: The CM3+ Lite brings the SD card interface to the module pins so a user can connect this to either an eMMC or SD card.
    • Environment: Operating temperature, -20° to +70°C
    • 35u hard gold plated IO Pins

     

    Buy the Raspberry Pi Compute Module 3+

     

    Without Flash Memory

    Raspberry Pi Compute Module 3+ LiteRaspberry Pi Compute Module 3+ Lite

     

    With Flash Memory

    Raspberry Pi Compute Module 3+ 8GBRaspberry Pi Compute Module 3+ 8GB

    Raspberry Pi Compute Module 3+ 16GBRaspberry Pi Compute Module 3+ 16GB

    Raspberry Pi Compute Module 3+ 32GB Raspberry Pi Compute Module 3+ 32GB

     

    Development Kit

    Raspberry Pi Compute Module 3+ Dev KitRaspberry Pi Compute Module 3+ Dev Kit

     

    Want to Discuss Raspberry Pi, Join Built Contents and Enter Give-aways?
    Check out the Raspberry Pi Space Here

     

    Why join the element14 Community?

    CONNECT. LEARN. CREATE. INSPIRE.

    Established in 2009, the element14 Community is the industry standard for electronics collaboration. It has popular technical blogs, videos and webinars that provide information on the latest in electronics trends such as the Internet of Things and Wireless Technologies. It also hosts our video project releases in element14 presents on Wednesdays and Fridays. It is a place where you can:

    • CONNECT with a community of thousands of engineers and innovators from all over the world.
    • LEARN about the very latest in new technology from industry experts, suppliers, independent sources and user reviews.
    • CREATE and source your next electronics project with access to 24/7 community support to tackle tough project challenges.
    • INSPIRE and be Inspired; build your next project and help others to create a better connected world.
    Our Exclusive Features

    element14 Design Challenge

    By connecting engineers to powerful new ideas and to each other, the element14 Design Challenge is creating innovative solutions to everyday problems.

    element14 Design Center

    Explore our huge selection of hardware development tools and software products, all supported with the technical resources you will need.

    EAGLE PCB Design Software

    Whether you are a team of one, or part of a large engineering department, EAGLE provides quality PCB design software with the features that get the job done.

    Join the ChallengeExplore NowLearn More

    element14 presents

    Join the hackers, engineers and makers of element14 presents as they tackle new and fun projects each week using circuitry design, 3D printing, microcontrollers, and much more.

    element14 RoadTest

    Apply to test new products from top manufacturers like NXP, Microchip, and Rohde & Schwarz. If selected, put that new product through its paces and you'll keep it for free.

    Online Learning

    Together with our manufacturer partners, we offer Webinars on a wide range of engineering topics. Stay up-to-date on the latest trends and the hottest technologies.

    Watch EpisodeEnroll NowStart Now

    Tech Connection

    Keep up on the latest tech trends with the element14 Tech Journal or learn about the most current technologies today in Tech Spotlight.

    Project14

    A monthly project compeition open to all Community members. Apply for a chance to win a $100 shopping spree.

    Prototype to Production

    Join element14's Business of Engineering and learn how to launch companies successfully from prototype to production.

    Learn MoreSubmit ProjectFind out More