Version 4
    Industrial Ethernet Quiz
    sponsored by logo name
    Quiz | Industrial Automation | Embedded | Internet of Things | Connectors Blog | Molex

     

    badge name

    How much do you know about industrial ethernet technology, protocols, and components? Take our quiz to find out.

    To earn the Industrial Ethernet Badge, score 100% on the quiz, rate this document, and leave your feedback on the quiz as a comment.

     

    1) Ethernet can replace what conventional technology used in traditional industrial networks?

         
         
         
         
       

     

    2) An end-to-end Industrial Automation Solution can incorporate which of these elements:

         
         
         
         
       

     

    3) Which of the following is NOT an Industrial Ethernet solution?

         
         
         
         
       

     

    4) For the industrial technology "Ethernet/IP" what does "IP” stand for?

         
         
         
       
       

     

    5) Which technology block is at the core of an industrial automation system?

         
         
         
         
       

     

    6) What is the benefit of gold-flash palladium nickel plated contacts on RJ11 and RJ45 modular jacks?

         
         
         
       
       

     

    7) Which organization manages the Ethernet/IP protocol?

         
         
         
         
       

     

    8) True or False: Brad Micro-Change (M12) Connectors have built-in strain relief to radiate stress in side-load conditions.

         
       

     

    9) A Molex Brad(R) IO-Link digital hub can offer up to how many connected devices at once, using a single PROFINET IP address?

         
         
         
       
       

     

    10) A Molex Brad(R) applicomIO Ethernet/IP network interface card provides connectivity for which of these:

         
         
         
       
       

     

    11) True or False: Molex's Brad(R) Ultra-Lock Stainless Steel Connection System creates a repeatable IP69K seal.

         
       

     

    12) What unique condition can an IP69K-rated connection withstand?

         
         
         
       
       

     

    13) True or False: Molex Brad(R) "Push-to-lock" connectors can be unlocked with a 4-digit PIN.

         
       

     

    14) True or False: Molex IP20 and IP67 Ethernet switches are PROFINET-compliant.

         
       

     

    15) Single Pair Ethernet (SPE) is different from traditional Ethernet's physical layer in what way?

         
         
         
       
       

     

    16) From the list below, which is NOT an advantage of Industrial Ethernet:

         
         
         
       
       

     

    17) Molex's industrial remote access solutions do NOT offer which benefit:

         
         
         
       
       

     

    18) Which is NOT an advantage of a Magnetic Jack?

         
         
         
       
       

     

    19) A Molex MXMag connector can support what maximum Ethernet speeds?

         
         
         
         
       

     

    20) Which is NOT true about the Molex Brad Micro-Change connectors?

         
         
         
       
       

     

    21) The Ultra-lock connection system from Molex can handle what maximum current?

         
         
         
       
       

     

    22) True or False: The Brad M12 Ultra-Lock Connection System offers push-lock connectivity, which means they cannot be used with traditional M12 threaded connectors.

         
       

     

    23) What are the two types of Ethernet/IP devices?

         
         
         
       
       

     

    24) Recessed pins within a die-cast shield offer what advantage?

         
         
         
       
       

     

    25) True or False: The Brad M12 Ultra-Lock 2.0 Female Cordset complies to the IEC 61076-2-010 standard and utilizes Weld-slag, oil-resistant (WSOR) cable to withstand multiple harsh-environment conditions, including welding and cutting oil.

         
       
    Alas, you didn't quite meet the grade. You only got %. Check out our resource doc and try again.
    You nailed it, and scored %! To earn the Industrial Ethernet Badge, leave us some feedback in the comments section and give the quiz a star rating.