Skip navigation
> Events

More Channels in Less Space: New Trends in Highly Integrated DACs

Event has ended

Loading...

Description

Enroll in the RoadTest: Quad-Channel, Analog Output Module

 

To download the slides please click here and sign into your myTI account or create a new one.

 

{tabbedtable} Tab LabelTab Content
About This Webinar

More Channels in Less Space: New Trends in Highly Integrated DACs

How a Highly Integrated Quad Channel Analog output module with Adaptive power management Solves the space demand problem in factory automation

 

 

Trends in the factory automation space demand that designers fit more channels in a smaller space. This means that systems are getting more dense, designers have to manage the system thermals better due to the need for high reliability, and efficiency is extremely important. This TI design addresses some of these key challenges by using a highly integrated quad channel 4-20mA and voltage output DAC with integrated adaptive power management. In addition, we will also discuss a reference design used to pass IEC61000-4 suite of tests.

tipd215a.PNG

This quad-channel, analog output module delivers voltage and current outputs using the highly integrated DAC8775 digital-to-analog converter (DAC). Integrated adaptive power management, along with the LM5166 buck converter, reduces the total power dissipation of the reference design to less than 1 W, even when driving all four channels at 20 mA simultaneously.

Webinar RecordingClick Here to Watch Webinar Recording
The Presenters

Tsedeniya_abraham.png

Tsedeniya Abraham is a product line manager in our precision DAC group. Prior to this role, she was the design manager for our industrial automation portfolio. She joined Texas Instruments in 2006 as analog design engineer.

 

kevin duke.PNG

Kevin Duke is a Systems Engineer in the precision digital-to-analog converters group at Texas Instruments where he is responsible for industrial automation DAC product definition and development. Previously he was an Applications Engineer supporting data-converters, focusing on DACs for Industrial Automation. Kevin received his BSEE from Texas Tech University in 2010.

Product FolderThe product folder for the EVM is here: http://www.ti.com/tool/dac8775evm. The GUI available there can interface with the boards for TIPD215.

 

Reference Design: Less Than 1-W, Quad-Channel, Analog Output Module with Adaptive Power Management Reference Design

This quad-channel, analog output module delivers voltage and current outputs using the highly integrated DAC8775 digital-to-analog converter (DAC). Integrated adaptive power management, along with the LM5166 buck converter, reduces the total power dissipation of the reference design to less than 1 W, even when driving all four channels at 20 mA simultaneously.

More info

Product folders:

  • DAC8775 - 16-Bit Quad-Channel Programmable Current-Output and Voltage-Output Digital-to-Analog Converter (DAC) -
  • LM5166 - 3V-65V Input, 500mA Synchronous Buck Converter With Ultra-Low Iq -

Applications: Analog Output Module

When and Where

  • Start Time:

    Jun 14, 2017 3:00 PM CDT (America/Chicago)
  • End Time:

    Jun 14, 2017 4:00 PM CDT (America/Chicago)
  • Location:

    webex

Event Info

  • Event Type:

    Webinar
  • Event Visibility & Attendance Policy:

    Open

Contact Info

Comments

Related Content