Skip navigation
> Events

Monarch Go Workshop: Part 2: Introduction to Azure IoT Central Out of Box Example

Description

An ideal starting point for LTE IoT application development.

 

The production-certified Monarch Go modem is end application certified allowing for easy transition from development to production.

 

Follow along with engineers from Avnet as they give you a hands on experience using  the Monarch LTE-M Development Kit, a cellular IoT enablement platform featuring the NXP LPC55S69-EVK and the Monarch Go Arduino Shield. The Monarch Go LTE-M modem component is perfectly suited for a broad range of IoT applications, including telemetry, vending machines, agriculture sensor applications, asset and transportation trackers, hardware tools, and home security monitoring applications.  Arduino form factor enables use with NXP EVK and third-party boards.  The Monarch Go Arduino Shield in conjunction with the LPC55S69-EVK is enabled with Microsoft Azure and AWS cloud support. The click module ecosystem enables sensors, interfaces, displays, motor controls and more to allow for thousands of LTE IoT development applications.  The Monarch Go Arduino Shield also has an onboard VEML6030 ambient light sensor and a SE050 plug-and-trust secure element. The availability of these capabilities on board enables prototyping of both motion and secure LTE applications out of box.The Monarch Go Cat-M1 modem delivers the shortest possible route to market and lowest development cost for cellular IoT-connected devices. Unlike traditional cellular modules, this modem is certified for use on the Verizon network, which avoids costly lab testing while improving time to market. The Monarch Go has an integrated antenna and pre-installed Verizon ThingSpace IoT SIM card, giving developers an easy, cost-effective approach to developing LTE IoT solutions.

 

 

Session 2:

 

In this session, we will discuss and setup an IoT Central cloud based embedded user example. This involves creating an interactive dashboard that displays telemetry as well as offers led control on the LPC55S69-EVK. Next application code will be edited with the users device credentials for proper handshaking and then built/deployed on the LPC55S69-EVK. Finally, will discuss how a user would take this out of box example and expand on the functionality of the out of box design.

 

Agenda:

  • Introduce IoT Central and the advantages powered by Azure
  • Discuss the Azure IoT Central Embedded code
  • Build and deploy the embedded code on your hardware
  • Showcase the functioning interactive IoT Central dashboard

 

To participate in this as well as the upcoming workshops you will need to purchase the following product online:

 

Required Hardware:

 

 

Development Environment Setup:

 

 

 

Dates and Register for Free:

 

Workshop:Dates and Time:

Session 1 - Deep Dive into the Monarch LTE-M Development Kit Advantage

Thursday, 10th of December 2020

 

11:00 CT / 4:00 PM GMT

 

Session 2 – Introduction to Azure IoT Central Out of Box Example

Wednesday, 23rd of December 2020

 

11:00 CT / 4:00 PM GMT

 

  • Register Above for Free!

Session 3 – Prototyping and Rapid Development using the Monarch LTE-M Development Kit

Wednesday, 6th of January 2020

 

11:00 CT / 4:00 PM GMT

 

 

 

Presenter:

Joshua Foster, Technical Marketing Engineer at Avnet
Technical Solutions Engineer (IoT / Avnet Products & Emerging Technologies) Lead engineer on multiple NXP-processor based platform development programs as well as Sequans Monarch Go Modem based add-on boards. (Based in Phoenix Arizona)

When and Where

  • Start Time:

    Dec 23, 2020 11:00 AM CST (America/Chicago)
  • End Time:

    Dec 23, 2020 12:00 PM CST (America/Chicago)
  • Location:

    On24

Event Info

  • Event Type:

    Webinar
  • Event Visibility & Attendance Policy:

    Open

Contact Info

Comments

Related Content