Skip navigation
Yes, the one on the far right. Replicator Z18 (via Makerbot) MakerBot, one of the leading manufacturers of 3D printers, recently announced that it has launched pre-order of its gargantuan Replicator Z18 3D printer, which is the best value for its size and performance, according to MakerBot.   The Replicator Z18 is the “mammoth” of all Makerbot 3D printers, enabling prints that are up to 18 inches tall. The printer sits at 19.4” W x 22.2” D x 33.6” H and ...
I just recently built my Printrbot Junior v2 3D printer and have been printing test pieces in order to calibrate the printer. Now that all that is done, and after printing a filament guide to keep my feed line under control I decided it was time to design and build something. I am attempting to build an Ironman MkIV suit for my son, and the arc reactor in the chest is one of the toy ones which light up and make a noise when you press the front. That was ok, but the lights were pathetic, so I ...

Filter Blog

By date: By tag: