Skip navigation
MIT has come up with a structure using just carbon which is ten times the strength of steel, but only 5% of its density. Lighter than air, 3D graphene structures could take engineering and design by storm. A 3-D printed model of gyroid graphene (via MIT & theregister.co.uk)   Steel has thus far been the gold standard for construction materials. Steel is strong, resists compression and stretching, and supports heavy weight. What if it were possible to build with materials even stronger ...
I find that the best projects start with a purpose, however what most people don't tell you is that the purpose doesn't always have to be prophetic, necessary or groundbreaking. For a lot of people starting a project can be as simple as the intention:   "I want to blink an LED"   When I joined Leeds Hackspace this was the first concept I was introduced to, along with the Arduino platform. This small and, to me, humble beginning has led me down a path which resulted in a change of job, ...
Chemists at MIT have found a way to add new polymers to things already printed, which allows them to create more complex objects that have different chemical and mechanical properties. Blue LED light is used to add monomers to an existing polymer chain resulting in growth. (via MIT)   Research funded by the National Science Foundation helped MIT researchers discover a way to add to, and alter 3-D printed objects after they’ve been printed. Until this advancement, objects that were 3 ...
Possibly the biggest growing technologie today is the 3D printer, this is partly due to its decreasing cost. This drop in cost of 3D printers is largely due to the standardization of the technology as more printers use the same base technologies. The cost of filament however, whether standard or exotic, still remain relatively high.   D3D Innovations has been working to change this. Their filament fabricators allow anyone to create their own filament using various plastics, combinations an ...

Filter Blog

By date: By tag: