Skip navigation

Azure Sphere

September 30, 2019
Please make sure Part 1, Part 2, Part 3 and Part 4 are correct before moving on to Part 5 below.     Section 5: Running the ShockDetect application!   5.1. Extract the attached zip file for this post to a directory of your choice. Make it a simple to type location, I recommend. Like C:\Shockdetect     5.2. In Azure Sphere Developer Console, navigate to that unzip location and run the ShowIoTCentralConfig.exe application that is located in Tools directory. You could a ...
Please make sure Part 1, Part 2 and Part 3 are correct before moving on to Part 4 below.   Section 4: Set up communication between Azure Sphere IoT device and Azure IoT Central Application. This communication uses certificates that were stored on HSM.   4.1. In Azure Sphere Developer Console download certificate from your Azure Sphere Tenant: azsphere tenant download-CA-certificate --output CAcertificate.cer   4.2. Upload certificate (Select All files (*) in upload window): ...
If you did not complete Part 1 and Part 2 successfully, go back and make sure it's correct.   Section 3: Create an Azure IoT Central Application.   3.1. Go to the site and log in using your Azure Active Directory Credentials: https://apps.azureiotcentral.com/create   3.2. Create application:   3.3. Create a Device Template:   3.4. Add the following telemetries: You have to add each of the following as a separate telemetry entry: acceleration_mg[0] acc ...
If you followed Part 1 without issue, move on to Part 2 below. If not, please go back and get Part 1 completely correct, otherwise it will have a ripple effect across the whole project.   Section 2: Now you can run your first application on your device in debug mode.   2.1. Put your device in debug mode: azsphere device prep-debug     2.2. Open Visual Studio:   2.3. Create New Project:   2.4. You can just Run Project on your Device: You should see t ...
Microsoft Azure is cool. It's an easy way to get an IoT project off the ground. The Azure Sphere Starter Kit is a great place to begin too. However, getting to that easy part is a journey. I've put together this guide to help people get started with a "hello word" kind of IoT project. I will step you all though the circuitous procedure of setting up a Azure account all the way through testing the project.   The project was a simple idea: detect vibration and send an alert. I want to do som ...